Part Number: TPS2595 We are using a TPS259571 efuse as an output load switch. We have a pullup resistor on the output so we can determine if there is a load present when the switch is off. My expectation is that when the eFuse is disabled, the output…
Part Number: TPS2595 Other Parts Discussed in Thread: BQ25672 Hi,
i am designing a power supply board for my irrigation controller. Attached you can find my schematic. The board is powered through a 12V LiFePo4 battery and a charge controller (BQ25672…
Part Number: TPS2595 Hi Team,
My customer is evaluating TPS25954 in their system, can you please check:
1.Do we have SOA diagram for TPS25954?
2.If Vout>Vin, do we have reverse damage on device? If so, does device be safe if Vout>Vin for about 2us…
Part Number: TPS2595 Hello,
I am using the TPS259531 eFuse and I am trying to determine the turn-on delay (tD,ON).
Input voltage (Vin): 3.3 V
Cvdt capacitor: 100 nF
VUVP: 2.54 V
Could you provide guidance on how to calculate tD,ON for these…
Part Number: TPS2595 Other Parts Discussed in Thread: BQ25672 HI,
i am deisigning an irrigation controller and I'm having problems with the power supply sections. The board will have a 12v LifePO4 battery that will be charged by a solar panel through…
Part Number: TPS2595 Hi sir,
what's the voltage level of TPS259541 ILM pin?
Datasheet doesn't mention.
Customer wants to use the voltage level for CPU use.
Part Number: TPS2595 Tool/software: Hi Expert,
Could you please provide the MTBF of TPS259541DSG and UL certification data for us ?
• UL 2367 Recognition – File No. E169910 – RILM >= 487 Ω (4.42 A maximum) • IEC 62368-1 Certified • Safe During Single…