Part Number: TPS272C45 I have been trying to simulate the TPS272C45DRHFR IC in PSpice for TI. I have added the library to my simulation profile, and the standard PSpice libraries are already added. I have also put the library in the project folder. Yet…
Part Number: TPS272C45 Other Parts Discussed in Thread: TPS281C30 , TPS27SA08 , TPS274C65 , TPS281C100 , , TPS274C65CP , TPS274160 Hi team,
Could you pls help recommend solution for below scenario
1. Normal operation range: 8-35v
2. No need to consider…
Part Number: TPS272C45 Other Parts Discussed in Thread: TPS4H160-Q1 , Tool/software: Hi,
Please provide the Demagnetization Capability for TPS272C45 same as TPS4H160-Q1 on Page 34 (Figure 4-5). Link : www.ti.com/.../slvae30e.pdf
Part Number: TPS272C45 Hi Team,
our cutsomer is Siemens and want to consult the value of max output leakage current for per channel in TPS272C45 when the Tj = 125℃.
There is only the value for the TJ=85℃ in datasheet.
It would be better if there…
Part Number: TPS272C45 kindly suggest suitable inrush current protection ic for 24v dc power which is used to drive led driver to drive vision mission led string.
also Need simulation file for TPS272C45 for specifically inrush current protection application…
Part Number: TPS272C45 Tool/software: Hi
The data sheet for the TPS272C45 states the maximum pwm frequency is 1khz, however Figure 7-12 show a pulse of 200e-6 sec. I am interested in the maximum pulse train, i.e. 50% duty cycle.
Thank you
John
Part Number: TPS272C45 hello
i would like more information about device TPS272C45ARHR. High side switch with VS tied to +28VDC and VDD tied to +5VDC.
i understand on datasheet that:
input pin EN1 or EN2 control each output OUT1 or OUT2.
when EN1…
Part Number: TPS272C45 Tool/software: Hello.
We use TPS272C45ARHFR component to drive some loads.
In the datasheet, we cannot find the minimum current in the load to avoid the "no-load" detection.
Can you provide us this parameter ?
Thank you…
Part Number: TPS272C45 Tool/software: I am operating the TPS272C45 in "Latch Off" mode (LATCH is high). After an over-current shutdown, how do I exit Fault Mode and return to Off, Diagnostic, or Active mode?
I've tried pulsing LATCH low for at least…
Part Number: TPS272C45 Tool/software: Hello, since I couldn't seem to find this information in the datasheet, I hope you can help me with this matter.
What is the accuracy of the current limiting in this device? The only points of reference I could…