Part Number: TPS3707 Tool/software: Hi team,
We want to promote the TPS3707-33DR to against STM708SM6F(ST), Is it a suitable device? if Yes, is there any difference between them.
BR
Jingguo
Part Number: TPS3707 Dear TI Team
Our customer is considering the TPS3707-50DR. However, when I look at the product page, I can't find the data sheet. Is it possible to get a data sheet? Best Regards,
Y.Ottey
Part Number: TPS3823 Other Parts Discussed in Thread: TPS3707 , TPS35 Hi team,
we want promote TPS3823 to fight with STM708SM6F, is it suitable? and is there any other suitable device we can promote?
BR
Jingguo
Part Number: TPS3707 Other Parts Discussed in Thread: TPS3808 Since the PFI/PFO feature of the TPS3707 looks like a simple comparator with a threshold of 1.25V, is there any issue with adding positive feedback from PFO to PFI to add external hysteresis…
Hi,
My customer has question about TPS3707-30. Could you tell me about question?
Question: If my customer doesn't use /MR function, how should he set /MR pin?
Best Regards,
tateo
Other Parts Discussed in Thread: TPS3707 Hello
This is a very specific question regarding the DGN package for the 3707. Does the PowerPad under the part connect to the GND signal of the part or what signal is the PowerPad connected to?
Part Number: OMAP-L138 Other Parts Discussed in Thread: CDCE906 , AM1808 , TPS3705 , TPS3707 , ADS1274
Hello,
we designed, and meanwhile produce, a DSP measuring system containing an OMAP-L138 CPU core system, which is a copy of the OMAP-L138 LCD KIT CPU…
Hi,
I do NOT have the datasheet of LP8765RLE, so I cannot confirm whether its RSTOUT_N (F4) requires an external pullup or not.
For the description on RESET (K14) in OMAP-L138, see Section 6.4.1 Power-On Reset (POR) & Section 6.4.2 Warm Reset of the…
Hi Matthew,
We currently do not have models for the TPS3707 family of devices. At the time that these devices released it was not common to release a model.
Very Respectfully,
Ryan