Part Number: TPS51215A Dear team,
Coud you pls recommend an automotive-grade low Vin BUCK (similar with TPS51215A but Q1 version), meeting the following requirements:
1. 2-bit VID control;
2. Output voltage: default 0.78V, adjustable to 0.95V/0…
Part Number: TPS51215A
Tool/software:
Hi
Could you help check the below TPS51215A schematic and any need to adjust
The inductor was 0.22uH with a DCR of 0.63mohm and was replaced with a 0.22uH with a DCR of 0.29mohm.
The inductor DRC is different…
Part Number: TPS51215A Tool/software: Hi,
Am I correct in understanding that by increasing the L constant from Equation 3 on p12 of the TPS51215A datasheet, the Iload(LL) point at which the auto-skip mode is entered can be lowered?
Also, am I correct…
Part Number: TPS51215A Hi,
I downloaded the PSpice Transient Model and am trying Sim. I thought that if the V0pin of the TPS51215A was set to a voltage other than 0V and the VID0pin and VID1pin were set to Low, a voltage other than 0V would be output…
Part Number: TPS51215A Other Parts Discussed in Thread: , TPS51518 , TPS54KC23 , TPS51219 Tool/software: Hi team,
I have three questions. Before asking the question, I will report on the evaluation environment and the evaluation results.
● Evaluation…
Part Number: TPS51215A Other Parts Discussed in Thread: TPS51518 Tool/software: Hi all,
I think TPS51215A and TPS51518 can switch the output voltage by 4 values with 2 bit VID function.
Is there no problem to use fixed VID and fixed output voltage…
Part Number: TPS51215A Other Parts Discussed in Thread: TPS51220 Tool/software: Hi,
In the datasheet, 7.3.6 Light-Load Operation gives the formula for calculating the load current at which the auto-skip mode is entered.
The TPS51215A enters auto…
Part Number: TPS51215A Tool/software: Hi team,
In the typical application diagram, the voltage divider line of VREF passes through V3, V2, V1, and V0.
However, if individual voltage divider circuits are used for each Vn pin, is it acceptable for the…
Part Number: TPS51215A
Hi support team.
Is it okay to recognize that the TPS51215A supports IMVP9? I found an example application for IMVP9 in the datasheet.
If this product supports it, is the answer to the following post incorrect?
https:…