Part Number: TPS51386 Hi team,
My customer has observed a phenomenon where the FB pin input voltage deviates from the set value, even though the values of the voltage divider resistors remain the same.
I would like to discuss this together with the…
Part Number: TPS51386 Tool/software: Hi Sir,
My customer is testing TPS51386 on thier product.
They want to eliminate radiation noise at 393.75Mhz and 684.75Mhz. Noise at 684.75Mhz has be limited by using RC snubber at SW pin (1nF+ 10R), but they…
Part Number: TPS51386 Other Parts Discussed in Thread: TPS51397A Hi,
Do you have TPS51386 thermal test data @8A(full load)?
Our customer is find for TPS51397A alternative but worry about the temperture.
Thanks!
Jeff
Part Number: TPS51386 Other Parts Discussed in Thread: TIGER , TPS51372 , TPS543620 Hi,
I am developing a SoM based on Intel Tiger Lake board and I am facing an obsolescence issue with the PMIC P8620 from Renesas which is Tiger Lake purpose-specific…
Part Number: TPS51386 Tool/software:
Here is my schematic, Vout and V_switching i just measured by oscilloscope. Load: Dummy load (Resistor = 4R) ~ 8W. From starting, i used Capacitor 22pF in compensation with 0R, i saw that output is very high peak…
Part Number: TPS51386 Other Parts Discussed in Thread: TPS51383 , Tool/software: Hello,
I have a problem that I would like to use this model in SIMPLIS/SIMetrix.
But it does not seem to support or read it for SIMPLIS/SIMetrix.
Could you please share…
Part Number: TPS51386 Tool/software: Hi Support,
Currently I have Design the Schematic
Input Voltage is 24V
Output Voltage is 5V
but i have get it 0.8V only at output point.
regards
Saurav
Part Number: TPS51386 Tool/software: Why is the DC voltage limited to 5.5V. I would like to design to 5.6V. Also, can I use the TPS51386 as an IBB to -5.5?