Part Number: AM5726 Hi Josue Zamitiz-Ayala
continuing the discussion from the attached thread.. ( https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1206364/am5726-cma_alloc-failed )
this problem started happening on the new…
Part Number: WL1831MOD
Hello,
I am currently having issues with the WL1831MOD. The modules seem to load just fine and the firmware that was generated from configure-device.sh is also loaded. However, as soon as a scan is initiated the driver appears…
Part Number: AM3352 Other Parts Discussed in Thread: WL1831MOD , I have a custom board that has an AM3352 and WL1831MOD on it, wired up exactly like the EVK and MOD8 board. It does seem to be mostly working but the data wlan interface seems very unstable…
Part Number: AM4378 Tool/software: We are working on am437x based custom board, Migrating from 4.19 to 6.1 kernel. I updated the dts changes specific to ethernet & cpsw switch taking am437x-sk dts as reference.
After updating my dts ethernet phy's are…
Part Number: AM625 Other Parts Discussed in Thread: DP83620 Hi,
i am using am625 hs-fs custom board based on processor sdk 8.06.00.042. could you any one suggest how to resolve the following kernel crash issue,
[ 11.264823] davinci_mdio 8000f00.mdio…
Hi Praveen,
As shown below:
I have check all CONFIG_USB_* entries in kernel3.14 configuration, They are the same。
kernel3.14 configuration:
#
# Automatically generated file; DO NOT EDIT.
# Linux/arm 3.14.63 Kernel Configuration
#
CONFIG_ARM…
Part Number: PROCESSOR-SDK-AM64X I am working on porting device trees from a device that was originally brought up on the 08.00.00.21 SDK So far I am able to boot and use the Ethernet device, but I do not see any PCI devices in `lspci` or in /sys
Diff…