Part Number: TPS54373 Other Parts Discussed in Thread: TINA-TI , TPS628503 Hello,
I am looking for the TINA-TI model for the TPS54373.
Specifically, I am looking for the Average Model.
There used to be models on the TPS54373 product page, like slvm299…
Part Number: TPS54380 Other Parts Discussed in Thread: TPS628513 , TPS54373
Hi Team,
We are using TPS54380 Voltage regulator in our design to generate 1.8V from 3.3V. Switching frequency is set to 700kHz.
Now the mentioned part is obsolete and hence…
Hi, John.
Please explain phenomenon of an attachment waveform.
-Why does movement stop suddenly?
-Why does a sink current flow?
-Why does it restart?
This waveform was observed customer's board.
TPS54373_StartUp_Failure.pdf
Part Number: TPS54610 Other Parts Discussed in Thread: TINA-TI , TPS54373 Hello,
I have a design that uses the TPS54610 with parameters used by Web Bench Power Designer for:
TPS54610PWPR ‑ 3V-3.4V to .95V @ 6A
The design uses parts found on our…
Sakai-san,
The TPS54373 is the version of TPS454310 that supports pre-bias. TPS54310 can operate in a pre-bias state, but it will discharge any pre-bias to ground during start up. If the pre-bias source is strong, extremely large sinking currents…
Other Parts Discussed in Thread: TPS54373 When powering up a C6454 device, suppose the power sequencing looks like this:
- 3.3V comes up first - 1.25V comes up next - 1.8V comes up last However, the 1.25V rail rises from 0 – 800mV in about 100us…