Part Number: TPSM8A28 Other Parts Discussed in Thread: TPS548A28 , TPS548A28EVM Hi Team,
My customer wants to use TPSM8A28 in their system as 3.3V power input condition. Do you think there are any risks such the use case? I can not check it on Webench…
Part Number: TPS568215 Other Parts Discussed in Thread: TPS54J061 , TPS54JA20 , TPS548A28 , TPS543B20 , TPS543820 , TPS543A26 Hi,
we are choosing part TPS568215RNNR for our design having following requirements,
1) For 3.3V output
Vin = 5V
Iout…
Part Number: TPS53319 Other Parts Discussed in Thread: TPS53515 , TPS548A28
Hi team,
I was curious, DCAP by definition should use vout ripple information directly from the output CAP, also DCAP2 need vout to generate ripple injection too.
but I…
Part Number: TPS548B28 Other Parts Discussed in Thread: TPS548A28 , TPS548A29 , TPS54JB20 , TPS54JA20 Hi
I would like to ask some questions about the TPS548B28 series
TPS548A28 TPS548B28 TPS548A29 TPS54JB20
1. In addition to the current, OCP, and…
Part Number: TPS53319 Other Parts Discussed in Thread: TPS548A28 , , TPS548A29 , TPS548B28 , TPS53318 Hi support team.
My customer asked me regarding behavior when VDD is 4.5V.
Recommended operating condition of VDD is 4.5V to 25V
In addition, Minimum…
Part Number: TPS53319 Other Parts Discussed in Thread: TPS548A28 , TPS53318 I need some help finding a replacement part for TPS53319DQPR.
Do we have anything P2P that can be used here with similar or better functionality?
I translated your question as the following.
" If 3.3V ± 5% is applied to the Vin terminal, is it necessary to apply an external voltage to the Vcc terminal?"
No, but to get the full load current, adding the external bias may be necessary.
See section…
Part Number: TPS548A29EVM Dear *,
please can you provide the PN for output capacitors ( C25, C26, C12, C13) because they are missing in SLVUBN8 - March 2020 ?
Also is it possible to provide Altium schematic and layout for this EVM?
Best Regards…
Hi Brian
Regarding TUSB8044, we are connecting to SMbus host of PCH, in case we need any modification.
For this pin (SMBUSz), I found the datasheet mentioned low for an I2C EEPROM and high for a SMBus host.
That's why we pull down this pin.
tusb4…