Part Number: TPS562231 Hi team,
My customer is considering adopting the TPS562231. During their evaluation, the following issue has been observed.
<Symptom> On the customer’s evaluation board, the input voltage of the DC/DC converter drops earlier…
Part Number: TPS562231 Hi team,
I have a question regarding the TPS562231. I understand that the actual behavior depends on factors such as input voltage and output current, but if a short circuit occurs between the following pins, there is a risk of…
Part Number: TPS562231 Other Parts Discussed in Thread: SN562231 Tool/software: hi,
SN562231 has been discontinued, can you still provide its datasheet? What is the difference between TPS562231 and SN562231?
Thanks!
Part Number: TPS562231
Tool/software:
We received 350pcs TPS562231 with DC 2320 from TI e-store. Could you pls help share the policy document for shelf life. We can find “ The minimum useful life of a TI product is based on the date of delivery to…
Part Number: TPS562203 Other Parts Discussed in Thread: TPS562231 Tool/software: This part has a newer version TPS562231. So seek you help to advise whether TPS562231 will go to EOL soon. If yes, pls help advise the plan.
Part Number: TPS562231 Tool/software: Hi,
I have following 3 questions about bode plot measurement for TPS562231
1. If we tried to obtain bode plot of TPS562231, Is it correct way below?
2. DCAP3 has one pole and one zero at low frequency to…
Part Number: TPS562231 We are analyzing below MPS DC-DC Converters. We need Rise time (tr) and Fall time (tf) of the MOSFETs in these DC-DC switchers.
TPS562231 and TPS560430T
Part Number: TPS562231 Hi team,
My customer have challenges for soldering TPS562231.
The IC is very light and it raises on soldering paste during melting process.
As consequence the customer often has pin 2 and 3 unsoldered.
Do you have any…
Hi Dsa,
TPS562231 couldn't pass EMI test, right?
TPS562231 schematic look well. would you like to share layout and SW waveform to do more analysis?
Please plot SW waveform without bandwidth limit. i would like to see if SW has ring and the the frequency…
Part Number: TPS562231 Hello,
We have used the following parts to create a power design for 12.6V to 7.4V and from 7.4V to 5V as well as 7.4V to 3.3V.
We need an engineer to review the design for us since we are facing some challenges under loaded…