Part Number: TPS61050 Other Parts Discussed in Thread: LM36010
Tool/software:
Dear Team I would like to design a circuit using the "TPS61050" BOOST LED DRIVER. I have a question about the waveform shown below in a BOOST type driver.
A pulse occurs…
Part Number: TPS61050 Hi Ti Team,
In our current design, we are using a TPS61050 LED driver for a light source. As per its datasheet in torch mode, we are able to provide up to 500mA current to the LED.
We are looking for an alternate part that can provide…
Part Number: TPS61050 Hi
Customers use TPS61050 to control Flash LED in PC CAMERA, the circuit is as follows.
LED_VCC supply voltage is 5V SDA, SCL, Flash_SYNC signal voltage is 1.8V When the power is found to be off, the LED will flash once.
When the…
Part Number: TPS61050 would there be any issues controlling colored LEDs with this controller? I notice in the description and datasheet, the part is specified for use with white LEDs but I would like to use RED and ORANGE.
I am looking for I2C controlled…
Part Number: TPS60150 Other Parts Discussed in Thread: TPS61050 目前的設定為: Flash on TPS61050_Data_00 = 0x90; TPS61050_Data_01 = 0x96; TPS61050_Data_02 = 0x00; TPS61050_Data_03 = 0xDF; FLASH_SYNC = High Flash off TPS61050_Data_00 =…
Part Number: TPS61050 Other Parts Discussed in Thread: LM36010 , TPS630242 , TPS63802 Hi Team,
We are designing a camera. In the same we are using flash LED also, and the operating temperature of DUT is -40°C to +85°C. We have worked on two different types…
Part Number: TPS61050 Other Parts Discussed in Thread: LM3405 , LM3414 Hi,
I am using TPS61050 in a Torch mode in my system design. I am able to provide up to 450-500mAmp current only, but my requirement is more than that. As per datasheet, TPS61050 Torch…
Part Number: TPS61050 Hi,
I'm using a TPS61050YZGR LED Driver and I would like to know if there's a special sequence for updating the
SAFETY TIMER, STIM[4:0] after device has been set in FlashLight Mode.
Datasheet says on page 28
"5-bit unsigned…
Other Parts Discussed in Thread: TPS61050 Hello
We have select TPS61050 in application and Cree LED as per below link and we need to interface single LED with TPS61050
We have following queries.
LED forward voltage is 3.3V and boost output is 4.5VDC…
Part Number: TPS61052 Other Parts Discussed in Thread: TPS61050 , TWL6037 , TPS65913 Tool/software: Linux Hi All,
I am working on TPS61052 flash light with linux-3.12. I have added platform data in device tree and compile the driver as a module.
I have added below tree structure …