Part Number: TPS61170 Hello. I have a battery-powered application where I need a 25V output rail. The control pin capability of the TPS61170 is highly desirable to reduce power consumption when the full 25V range is not needed. 25V from a 3V battery is…
Part Number: TPS61170 Hello. I have a battery-powered application where I need a 25V output rail. The control pin capability of the TPS61170 is highly desirable to reduce power consumption when the full 25V range is not needed. 25V from a 3V battery is…
Part Number: TPS61170
Background: Our customer is planning to use the TPS61170DRVR as a phantom power supply block. The datasheet lists VIN = 4.5 V to 15 V as the recommended operating input range(p22). They would like to evaluate the device at input…
Part Number: TPS61170 Tool/software: Using the unchanged TPS61170EVM-280 changing the FB voltage using PWM on the ctrl pin does not seem to work
PWM freq : 6 kHz, DC : 90%, 5Vpp, offset 2,5V.
Input voltage 10V.
expected FB voltage : 1.229*90% =…
Part Number: TPS61170
Tool/software:
Hello,
I want to have 3-12v input to 3-12v output sepic regulator at maximum of 300-400 mA current, adjustment is via potentiometer. I saw this device which looks promising and cheap enough but I have these…
Part Number: TPS61170 Other Parts Discussed in Thread: TINA-TI Tool/software: Hi
i have create a simple design with TPS61170 boost on TINA-TI simulator.
But when i try to go to "Analysis -> Transient" i receive an error and i can't continue.
It…
Part Number: TPS61170-Q1 Tool/software: Hi experts,
I designed a negative voltage circuit based on the charge pump topology.
The load capacity of the circuit confuses me: We use a constant current source to extract the load. the -24V output can drive…
Other Parts Discussed in Thread: TPS61170 I'm trying to take a +9VDC and output a -9VDC with a load of approximately 100mA. My simulation works as expected. However when transferred to a PCB layout it is not working correctly. On the PCB bench testing…