Part Number: TPS61170-Q1 Dear support team,
I would need a better understanding of the VREF drift of TPS61170-Q1. In our datasheet we specify @ Vin=3,6V , CRTL=Vin, VREF with 1,204Vmin, 1,229Vtyp, 1,254Vmax.
The use case will be Vin = 5,4V, CRTL = 2,5V…
Ed,
The TPS61170/-Q1 loop and efficiency models may not work properly for very light load like the value you are specifying as the DCM operation is not modeled for these devices. The design for the TPS61170-Q1 could, however, be used instead of the TPS61170…
Other Parts Discussed in Thread: TPS61170-Q1 , TPS61170 Hi Team, There is difference of thermal resistance value between old datasheet and revised. Could you tell me the background of the difference? (SLVSAX2 –SEPTEMBER 2011) (SLVSAX2A –SEPTEMBER 2011…
Part Number: LM5157-Q1 Other Parts Discussed in Thread: TPS61170-Q1 , LM5158-Q1 , LM5158 , TPS55332-Q1 Hi, TI Support Team
I have received a request to recommend replacement parts for the following parts from a customer.
Please refer to the detailed spec…
Part Number: LM2623-Q1 Other Parts Discussed in Thread: TPS61089 , LMR62014 , TPS61170 Hi,
I am currently using the LM2623-Q1 in one of my design with the following requirements:
- Vin [6;8.4V]
- Vout 12V
- Load: <= 0.4A
I followed the reference design…
Part Number: TPS55340 Other Parts Discussed in Thread: TPS61175 , TPS55288 , TPS61378-Q1 , TPS61170 , TPS61391 , TPS7B4253-Q1 Hi,
We are using TPS55340 for boost converter. During the test, it has very high ripple for our design. Our schematic is shown as…
Part Number: MC33063A-Q1 Other Parts Discussed in Thread: TPS61170 Hello,
For the part MC33063A-Q1, my input will be 5 V ? I want to achieve a boost output of 36V or higher. Is it achievable ?
This issue is related to ton,toff ratio. For a 36V output…