Part Number: TPS61181A Hello,
Our customer ask us about the behavior when a string is open.
Please see attached file and give us your opinion/advise.
Thanks and best regards,
Hiro
TPS61181A_inquiry.pptx
Part Number: TPS61181A Hello,
I'm trying to use two TPS61181A to drive one LP097QX1 Display. (12 Strings)
LED-Anode 1 and 2 are presumably connected in the Display Unit.
The Problem I'm facing is that the Lighting works for about 1/2 to 1 Second before…
Other Parts Discussed in Thread: TPS61181A , WLEDEVM-260 Hi,
May I know how can implement TPS61181A EVM with WLEDEVM-260 for 3~6 LEDs Series function verify as using Fig.22?
Now the EVM can't workable with the below schematic.
Please kindly provide…
Hi,
With Analog+PWM, it's fine to continue using TPS61176.
For other devices, I'd like to recommend TPS61181A.
it has the same package (but not pin-to-pin) with TPS61176
support PWM dimming with brightness range from 0% to 100%
6 channels…
Hi ram,
Unfortunately I am not familiar with the TPS61181A, but I will go ahead and move this thread to the backlighting group where the device experts can help answer your questions.
Regards,
I.K.
Hello Hank.
Thank you for reply.
I try to check his Matter.
"I think there is about 6 or 7 LEDs in LED1 and LD2, then i have a guess want to check, if increase the LED number to 10, then how about the result?"
At the same,I want you tell me…