Part Number: TPS61299EVM-016 Other Parts Discussed in Thread: TPS61299EVM-103 , TPS61299 Hi Team,
May I check what is the difference between TPS61299EVM-016 and TPS61299EVM-103?
Thanks!
Part Number: TPS61299EVM-103
The quiescent load turns out to be way larger than 95 nA, it sums around 500 nA with a high fluctuation of +-3uA. According to the datasheet, it should be 95nA (as in the datasheet characterization plot).
The output being…
Part Number: TPS61299EVM-103 Hi team,
A customer is looking into the TPS61299EVM.
The EVM is operated under the following conditions:
Input voltage: 1.0V
Output voltage: 3.6V
Load current: approximately 10uA
The EVM is operated in PFM mode.
At the input…
Hi Dahan,
No, If you need TPS612997, you need to apply for TPS61299EVM-103 and TPS612997 samples. The default IC on TPS61299EVM-103 is the 1.2A current version TPS61299 so you need to apply for TPS612997 samples and replace the IC.
Best Regards,
Travis
Part Number: TPS61299 Hi, We are considering the use of TPS61299 for our product and I have tested the TPS61299EVM-103 with our load and it seems to work fine. But in the datasheet it is written that the chip can output 500mA with 3V to 5V input and limit…