Part Number: TPS62090-Q1 Support Path: /myTI & TI store/myTI account/ Hello,
I like to find out what will be the load in mA for this device to enter DCM mode?
Also, I like to know should I increase the power inductor in order to decrease the load…
Other Parts Discussed in Thread: TPS62090-Q1 Hi, Could you tell me about TPS62090-Q1 Fsw? Customer is using the TPS62090-Q1 at 2.8MHz setting and following conditions. ◇Vin=5V、Vout=3.3V、Iout=2A In the above case, Switching frequency works with the value…
Part Number: TPS62090-Q1 The EN pin has an internal pull down resistor of 400Kohm,. The DS shows example of directly pulling up EN pin to the supply. Do I need an external 100Kohm to pull up EN pin or directly connected to the supply with no pull up resistor…
Other Parts Discussed in Thread: TPS62130A-Q1 , TPS62090-Q1 Hi, Team
An answer is demanded from my customer for Machine Model ESD.
Do TPS62130A-Q1 and TPS62090-Q1 have a standard for Machine Model ESD ?
In addition, Does the ESD meet 200V ?
…
Other Parts Discussed in Thread: TPS62090-Q1
IC
TPS7B6333QPWPRQ1
TI
TPS7B6333QPWPRQ1
IC
LM63625DQPWPRQ1
TI
LM63625DQPWPRQ1
IC
TPS74518PQWDRBRQ1
TI
TPS74518PQWDRBRQ1
IC
TPS62090-Q1
TI
TPS62090QRGTRQ1
…
Hi
Do you see the similar issue on other margining rail other this BMC1V15? All margin voltage will tingle.
Have your checked whether TPS62090-Q1 allow adjust FB voltage externally? yes.
if you do not set the margin mode to active-trim, instead…
Hi Shyama,
According to your description, the application required only one buck. I think TPS62090-q1 will fit in your application. Could you explain why you want to use the dual converter?
Best regards,
Tanvee