Part Number: TPS62130A-Q1 Tool/software: Hi All,
I am using the TPS62130A-Q1 PMIC to power a 1.1V chip. I would like to have a voltage configuration option for this PMIC using a digital potentiometer.
The equation below can be used to calculate the…
Part Number: TPS62130A-Q1 Tool/software: Dear Experts,
Please help review the attached schematic using TPS62130A-Q1 to supply 3.8V for GSM module power. Input: 5V Output: 3.8V Is the feedback and soft-start network correctly configured?
Appreciate…
Part Number: TPS62130A-Q1
Tool/software:
I'm looking for the Failure Mode Distribution(FMD) and Component Failure Rates per Siemens Norm SN 29500-2 for this device, this is usually contained in a Functional Safety report (See https://www.ti.com/lit…
Part Number: TPS62130A-Q1 Other Parts Discussed in Thread: TPS62130 We have estimated the power dissipation on the TPS62130A-Q1 mounted on a 10-layer HDI PCB as 0.7W based on measured data.
The thermal resistance parameters mentioned in the datasheet…
Part Number: TPS62130A-Q1 I setting the switching frequency as 2.5MHz.
but why in my measurement the maximum switching frquency only 1.56MHz.
for variable switching frequency, how can I calculate the indutance?
my condition:
Vin=8V, Vout=1.09V…
Part Number: TPS62130A-Q1 Hello,
I was asked to perform bode tests on a board with the component listed above. I was wondering if DCS devices such as this can even obtain valid network analyzer results. The plots I have taken appear valid, but I wanted…
Part Number: TPS62130A-Q1 Other Parts Discussed in Thread: TPS62903-Q1 , Hello TI Team,
We are using TPS62130AQRGTRQ1 in our design and having following observations:
1. We are having an application of converting the 5V input to 3.3V output. The inductor…
Part Number: TPS62130A-Q1 Hi, Expert:
I found TPS62130A-Q1 datasheet Figure-50 1.8V 3A application FB pin R1 /R2 resistor were 360K/160K , the Vout=2.6V not 1.8V with VFB=0.8V in the datasheet page 28. Figure 50.
can you check the figure have something…
Part Number: TPS62130A-Q1 Hello Support,
I have seen the reference design of TPS62130AQRGTRQ1 and want to convert 12V to 5V,3A output.
Since it is a buck convertor what minimum input current is required with 12V input voltage?
Since it is not…