Part Number: TPS62136 Tool/software: I would like to get a TI Apps engineer to review our schematics for Lockheed martin. Lockhead Martin has an NDA/PIA in place with Texas Instrument. The Schematics are not classified but they are ITAR, It is just LDO…
Part Number: TPS62136 Hi E2E,
Can you provide a device which is 5A and similar with TPS621361?
The package size is similar and if there's P2P solution is better.
Part Number: TPS62136 Hi TI,
For the TPS621361 chip, I want to enable this supply from a system on a module that outputs a 3V3 signal via GPIO. All documentation for this chip suggests always tying it to the Vinput line. With the implementation I…
Part Number: TPS62136 Hi Team,
The datasheet for the TPS62136RGX only includes the max height and not the typical/min spec. Our customer needs this information, and I wanted to see if this is something we have on hand?
Regards,
JP
Part Number: TPS62136 I am powering DDR4 memory with a TPS62136. The output voltage is 1.2V. The inductor is a Coilcraft XGL4020-222MEC, 2.2uH, 20mohm. The output capacitors are a pair of GRM31CR60J476ME19L, 47uF, X5R, 6.3V, 1206. As the transient test…
Part Number: TPS62136
Hi, I will use TPS62136 for 5G Module. In the example power diagram in the 5G Module HW Design Guide, it is recommended to use 2 x 220uF capacitors at the module input. Reference circuit: https://drive.google.com/file/d/1CRF08FVHV61a5waHIUr0RnXt7wvWT8UJ…
Part Number: TPS62136 Hello TI
The data sheet for the TPS62136 suggests that in order for the voltage output to be stable the total ESR of the cap bank can't get too low. For a power rail capacitance of >= 400 uF, it is recommended that that the trace…
Part Number: TPS62136 Other Parts Discussed in Thread: DAC8734 , TIDA-01423 , , LMR33640 , TPS62933 Hi TI experts.
I need to design from a 5V input a -12V output to be fed to the negative rail of the TI DAC8734.
So I have taken as a starting point…
Part Number: TPS62136 Hello,
Our PCB currently has 2 of the Buck Converter Circuits below. Both VIN nodes of the buck converters are connected to the common port of a SPDT Relay. This SPDT relay serves us our power path to select either the battery…
Part Number: TPS62136 Other Parts Discussed in Thread: TPS62135 , TPS62902 , TPS62903 Dear support
The 3-17V 4.0A Step-Down Converter TPS62136 seems to be not available at the moment.
Is there any rough estimation, when the TPS62136 is available again…