Part Number: TPS62160-Q1 Other Parts Discussed in Thread: TPS62170-Q1 Dear TI Team,
I'm looking for a potential alternative for TPS62170-Q1. TPS62160-Q1 seems to be a promising candidate.
When comparing both datasheets the only difference I could…
Part Number: TPS62160 I am using TPS62160DSG in my EVSE design. I am providing 12V as input and I want 5.1V as output. To get 5.1V output I have adjusted the feedback resistor but still I am not getting 5.1V and sometimes I am getting 4.98V as output…
Part Number: TPS62160 The application issues of chips
The schematic diagram of TPS62160DSGR is attached
I'm consulting about the high standby current of TI DCDC devices
The circuit and parameters are basically in accordance with the specification…
Part Number: TPS62160 Tool/software: need help with web bench tool. I have temp set to -40C with custom resistor value set to 6.8599 K. Sim runs well.
I now want to run sim at 20C. I change temp from-40C to 20C, then the tool resets my custom resistor…
Part Number: TPS62160-Q1 Tool/software: Hello! I'm using TPS62160-Q1 in one of my boards to generate a 5V output from 12V input. I've built the circuit to look like this one in the datasheet, changing the values of inductor and FB resistors to match the…
Part Number: TPS62160 Tool/software: Hello, My customer has some questions as follows. Q1: Regarding EN rising time, how slow it could rise? Are there any slew rate (V/us) spec? Q2: When Vin ramps up, if Vin is < the minimum falling input voltage 2.6V…
Part Number: TPS62160 Tool/software: Hello TI support team,
Is there a way we can track down wafer ID/traceability from the top marking in your devices?
Some examples would be MPNs:
TPS62160QDSGRQ1
5432A0GPAANRQ1
Thanks,
Arturo.
Part Number: TPS62160 Tool/software: How do I calculate the conversion efficiency of a DC/DC converter? For example, when choosing a 1.8V voltage regulator chip between the TPS62160 and TPS7A0518, I want to minimize the system’s power consumption. I’m…