Part Number: TPS62177 Hi,
I am using the TPS62177 powerd from 24V, output 3V3. Input capacitance 10uF and output capacitance 30uF. PCB Layout equal to the layout recommended in the datasheet. The device powers a microcontroller withe reset controller…
Other Parts Discussed in Thread: TPS62177 For the TPS62177, is the design inherently low enough of a radiator such that using the recommended layout and inductor[s] will typically pass FCC unintended radiation requirements or do most designs using this…
Other Parts Discussed in Thread: TPS62177 I have a question about TPS62177.
Please tell me minimum,typical and max input impedance of EN pin.
Best regards,
Part Number: AM2434 Other Parts Discussed in Thread: TMDS243EVM , UNIFLASH , TPS62177 , I am trying to flash TMDS243EVM using mcu_plus_sdk_am243x_08_06_00_45. However, writing fails as shown in the screenshot. Using the same script to burn TMDS64GPEVM is successful…
Other Parts Discussed in Thread: TPS62177 I have a question about EN pin impedance of TPS62177.
My customer trys to put the resister between VIN and EN pin to delay startup time.
Please tell me typical ,max and minium impedance of TPS62177 EN pin.
And…
Other Parts Discussed in Thread: TPS62177 Hi with the help of WEBBENCH I have painted an implementation. For C1, C2 and L1 I used the values recommende by WEBBENCH (2.2uF, 22uF, 10uH). Input is 17V to 18V and current bewenn 100 mA in standby and around 400mA…
Other Parts Discussed in Thread: TPS62177 Hi,
I'm designing with the TPS62177 to generate an output voltage of 3.3V. At normal operation, the consumption is about 10 mA. One thing that I didn't notice is that I've left the SLEEP pin unconnected.…
I followed a design on Webench to convert 24 Vdc to 3.3 Vdc.
Schematics is the same but changed the layout a little bit
I am having a serious problem on the highlighted part (24V in), my modules are fried up, I often see a flame. I tested 20 modules…
Other Parts Discussed in Thread: TPS62177 Hello,
Can i please post here my TPS62177 schematic for review of my schematic & components choose ?
Regards,
Eduard