Other Parts Discussed in Thread: TPS62177 , TPS62175 Hi,
We are looking at using the TPS62177 in a design.
It will maily be used as a step-down DC/DC from 9-26V to 3.3V. Max load is about 500mA.
Another input voltage we would like to support is 3.3V (we…
Other Parts Discussed in Thread: TPS62177 Hi,
I plan to use the TPS62177 (Vout = fixed 3.3V) in a configuration where Vin is 9-26V.
I would also like to be able to supply this board with 3.3V directly when the 9-26V input is floating (not connected). That…
Other Parts Discussed in Thread: TPS62177 Circuit problems occurred during testing.
TPS62177 -> Fixed Output : 3.3V/500mA
But 3.3V is not output when configuring following circuit.
In -> 8V, Out -> 1.8V
In -> 12V, Out -> 3.5V
In-> 20V, Out…
I'm using a TPS62177DQCT 3V3 fixed output regulator. I used the schematic below.
When I connect a resistive load of 6.6 Ohm (500mA), and then apply VIN of 24V, the Vout rises to a stable 2.9V. Only after removing the load for a split second, the Vout…
Other Parts Discussed in Thread: TPS62175EVM-098 Part is here – http://www.ti.com/product/tps62177
The data sheet is very vague on how to identify pin 1. We are trying to verify that parts are mounted to a board correctly. What mark should we be looking…
ok so I am at a loss on this.
I have a small power adapter board to take 19V down to 3.3V. when I apply power to it the first time, it powers up fine and produces 3.3v, however when i disconnect power and reconnect it, the chip literally blows a hole…
Other Parts Discussed in Thread: TPS62177 Hi,
I'll use TPS62177 in a project. I'm using the Webench tool to check BOM and features etc.
I'd like to export the schematic to Cadsoft Eagle Cad 6.4 but there is an error:
ERROR: Exception occured…
Other Parts Discussed in Thread: TPS62177 , TPS62175 Hello, I am having trouble with TPS62177 (DQC). It operates from 5V to 12V, but when I tried to raise the voltage further up, the simple power supply broke, keeping the output at zero, but consuming significant…
Hi Michael,
Are you referring to https://www.ti.com/lit/df/tidrx16/tidrx16.pdf?ts=1596511941095&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FTIDA-050012 ?
This shows a TPS62177 device supplying VIN_3V3.
Can you please point your customer to this…