Part Number: TPS62442-Q1 Hi Expert,
Have a nice day! I have question need your professional support:
1. About TPS62442-Q1’s EN pin, What is the schematic inside it?
2. Besides the voltage threshold, does it have Min/Max input current request?…
Part Number: TPS62442-Q1 Other Parts Discussed in Thread: TPS62442 Tool/software: Hi,
How can we start different times two output of the TPS62442? When we put on different capacitor EN1 and EN2 terminals to gnd, It can not run on pspice for TI tool…
Part Number: TPS62442-Q1 Tool/software: HI friend,
May I ask if this design proposal is okay?(Including the selection of resistors, capacitors and inductors)
use condition: Iout1(typ)=534mA;Iout1(max)=1780mA; Iout2(typ)=748 mA;Iout1(max)= 1136 mA
Part Number: TPS62442-Q1 Tool/software: Hi,
I want to use large output capacitance and also i want to use this regulator with adjustable switching frequency. I understand that i can achieve both of them with comp2 setting and ssc disabled version so…
Part Number: TPS62442-Q1 Hi team,
Can you please help review the Pateo TPS62442QWRQRRQ1 SCH as below? Thanks
TPS62442QWRQRRQ1.pdf
Best Regards,
Xiaowei Zhang
Part Number: TPS62442-Q1 Tool/software:
HI friend,
May I ask if this design proposal is okay?(Including the selection of resistors, capacitors and inductors)
use condition: Iout1(typ)=534mA;Iout1(max)=1780mA; Iout2(typ)=748 mA;Iout1(max)= 1136 mA…
Part Number: TPS62442-Q1 Tool/software: Hi Expert,
Have a good day!
About TPS62442-Q1’s MODE/SYNC Pin, when MODE/SYNC is pulled up/low, user can set the mode.
My question is what is the control mode when MODE/SYNC pin connect to external frequency…
Part Number: TPS62442-Q1 Tool/software: Hi Expert,
Hope you have a good day!
About TPS62442-Q1,
Why the comp setting 1’s output capacitance is smaller than comp setting 2?
What is the internal circuit difference between comp setting 1 and…
Part Number: TPS62442-Q1 Tool/software: Hi Expert, I am also facing similar issue as this thread : -Q1: Regarding Rcf at COMP/FSET - Power management forum - Power management - TI E2E support forums for calculating Rcf in comp setting 1 with SSC enabled…