Part Number: TPS62827
Tool/software:
Hi TI experts,
I notice that the low side of input capacitors and output capacitors are routed together in layout guidelines.
Can the low sides of these capacitors be routed to the ground plane through separate…
Part Number: TPS62827 Dear Team,
Measuring the Noise at the 0.8V step-down output of TPS62827DMQR VSON-HR-6 is about 120mV on average. Correcting the capacitance value at the output has no obvious effect. How can it be improved?
In the attached…
Part Number: TPS62827 Tool/software: Hi All,
In tps62827 datasheet, there are only discharge current.
How to find out the output discharge current ?
Can I use V=IR to get the output discharge current ?
=> Rdischarge = 0.4v / 75mA
Thanks…
Part Number: TPS62827 Tool/software: Hi team
Attached image is the waveform of TPS62827 Enable pin. Negative voltage reaches to -0.5V that is lower than abs max rating. The pulse duration is nsec order. Do you this is violated to abs max rating? It…
Part Number: TPS62827 Other Parts Discussed in Thread: TPS62826 , , TPS62824 , Tool/software: Hi team,
Customer evaluates both TPS62826 and TPS62827 and found there are different perfromance.
For example, the bode plot with VIN=5.1V, VOUT = 1.5V,…
Part Number: TPS62827 Other Parts Discussed in Thread: TPS62868 , TPSM82866C Tool/software: Hi,
We want set 2 output voltage level 2.1V and 2.5V. We using N-MOS in parallel the resistor on FB pin, is it may have any side effect? thanks!
Part Number: TPS62827 Tool/software: Hi expert,
Customer used TPS62827 for 4Vin to 0.85V/4A application and have a question regarding Fsw. They want to know if any problems from their design.
They did test to measure Fsw in different loads. Our DS…