Hi Rajesh,
I have looked into the thread that you are referring to, It looks like they provided the requested values using the simulation.
I know how to get the values when we have SIMPLIS model for this device, but unfortunately we don't have SIMPLIS…
Part Number: TPS62822 Other Parts Discussed in Thread: TPS628502-Q1 Tool/software: I inquire about the functional safety FIT(Application FIT Rate) value and failure mode distribution, Gate scale for TPS62822.
Standard is SIEMENSE SN29500-2.
(it is…
Part Number: TPS628503-Q1 Other Parts Discussed in Thread: TPS628502-Q1 Tool/software: Hi Team,
Do we have a PSPICE model for the TPS628503-Q1 ? Please share if available.
Thanks in advance!
Part Number: TPS628503 Other Parts Discussed in Thread: TPS628502-Q1 , Hi team,
How to understand the junction temperature for the TPS628502-Q1 and TPS628503-Q1?
Is the Tj 105 °C for TPS628502-Q1 in continuous output, too?
BRs, Haury
Hi JH,
Thanks for reaching out to us.
I recommend TPS628502-Q1 if SOT-563 package is fine with customer. If not, TPS62812-Q1 (QFN package) is alternative choice as well. TPS628502-Q1 is a cost-competitive compared to TPS62812-Q1 due to higher Rdson…
Hi Miyaoka-san,
Please refer to the efficiency data of TPS62065-Q1 below. However, the efficiency at ~150uA load is around 55% only. If the customer needs a much higher efficiency at light load, we can promote TPS628502-Q1, which has a ~75% efficiency…
Hello Mingkang,
I have tested on TPS628502-Q1 but it is same family but just rated at 2A and there should not be any difference in terms of short circuit behavior.
Thanks,
Farheen
Part Number: TPS62A01A-Q1 Other Parts Discussed in Thread: TPS62A01A , TPS628502-Q1 , Hi team,
Do you have PSRR value from f = 10 kHz to f = 20 MHz?
Best Regards,
Shoji
Hello ,
We do not recommend using values above the mentioned values in D/S as device is validated only with that. It can affect the stability performance.
R values, you can choose according to resister divider equation: Vout=(1+R1/R2)x0.6
Capacitors…
Hi Rakesh,
Unfortunately, we do not have the PSpice model for TPS628503DRLR. But we have the Webench for simulations.
Alternatively, I suggest to use PSpice for TPS628502-Q1 for your evaluation. They differ by max current.
If required, you can also…