Part Number: AM6546 Other Parts Discussed in Thread: TMDX654IDKEVM , TPS62864 Hello,
is it possible to change clock freq to 1G or 1.1G at TMDX654IDKEVM eval board?
I tried to change the clock freq in .dts file, like found here
https://e2e.ti.com…
Hello Arumugam,
Can you have a look at the TPS62864 ? It has an I2C adjustable output voltage from 0.4V up to 1.675V in 5mV voltage steps.
QFN spin of this device will soon be available in preview.
Are you willing to consider I2C for your design…
Part Number: TPS62363 Other Parts Discussed in Thread: TPS62864 , TPS62866 Hi,
Could you please help for below question about TPS62363.
Below figure is on the page 15 of the datasheet of TPS62363.
Why there is a voltage step on Vout? Could you…
Hello Dorian-san,
Thanks for the information. I will let customer know the Fig 11 to 14. If you also have more detail about the accuracy in PFM, could you provide me it?
Thanks for the proposal of TPS62864. I will propose it to the customer.
Regards…
Part Number: LM3242 Other Parts Discussed in Thread: TPS62864 , TPS62800 I have to turn on the system at -40C and operate within 1 minute without external heating. Since the part is operational temperature of -30C min does the output gain go higher than…
Thank you for perfectly explaining.
We have the I2C-controlled TPS62864, but this comes in a WCSP package and does not support 2Vout.
You could do your method with the TPSM82822, but you cannot achieve the 0.55V since this is below the 0.6V FB pin…
Hi Kazuki,
The limitations for the start up sequence are determined by the absolute maximum voltage values in the table on page 2 of the datasheet.
According to this table, if pin AVIN is connected to VIN, then having EN at a higher voltage than AVIN…
Hi User,
Dorian is out for a few days, but let me comment until he returns.
The reason for the small increase in frequency from 1A to 4A is as it is explained in the app note:
In Figure 2a, the frequency increases with heavier loads due to losses…
Hi,
At datasheet of TPS62410, If the customer use EasyScaleTM One-Pin Serial Interface for Dynamic Output Voltage Adjustment, Vout1 output is up to 1.575, Vout2 output is up to 3.3V. is it right? - Correct
Are you looking for a dual converter with…