Part Number: TPS62876-Q1 Other Parts Discussed in Thread: TPS62870-Q1
Hi engineer:
about power design issues for TPS6287X-Q1:
In stacked operation mode, does it support DVS adjustment? How is the voltage adjustment of the Secondary achieved? How…
Part Number: TPS62868 Other Parts Discussed in Thread: TPS62870-Q1 Hi,
Does TI have I2C buck with PGOOD and slave address can adjust?
TPS62868 seems can't both have PGOOD and VSET function to adjust I2C slave address.
Application is Vin= 3.3V to…
Hi Chris,
I assume Vfb in the (1) formula is fixed at 0.6V, is it correct ?
If my load is purely resistive, won't my control voltage I apply with the DAC also depend on the load's current value ?
I wish TPS62869 and TPS62870-Q1 were available but…
Part Number: TPSM82866A Other Parts Discussed in Thread: TPSM82823 , , TPS62870-Q1 Hi Expert,
My customer have question about TPSM82866A and TPSM82823. They used TPSM82866A and TPSM82823 in new project. But output current design change, they have to…
Hi Shifali,
Our TPS62870-Q1 should be on the web in the next few days. It can operate from 3.3Vin. You can parallel 2 or 3 of them to get your 30-35 A.
Chris
Hi Shubiao,
Thanks for your question.
As specified in the datasheet, "The output voltage can be stepped down to as low as the 0.799-V reference". You can just connect Vsense to Vout.
Please pay attention that this device is a last time buy. The…
It all depends on your end product requirements & desired feature set. Please see J784S4 Power Solutions slide set to determine your optimal PDN-3x scheme. Once the scheme is determined, then the PDN power resources & mapping have been set to minimum…