Thanks for the reply.
I failed to mention in the original post that the power solution is for DM368+peripherals. We cannot use TPS650061 as the current requirement exceeds 300mA provided by LDOs.
Both TPS65023 and TPS650532 matches the requirements (TPS650523…
Hello Alex,
I have TPS650061 (Power Management IC) on my board. When I connect 1- pin (Manual reset) to GND I have reset on pin-20 (Open drain active low reset output), but Power is not OFF and than ON. Is this a correct ?
Yes, it is an expected behavior…
Hello Amit,
TI recommends to use TPS650061 for powering the OMAPL138 device. You can refer the below document for more details.
http://www.ti.com/lit/an/slva513/slva513.pdf
Regards,
Senthil
Other Parts Discussed in Thread: AM1808 , TPS650061 , OMAPL138 Using a AM1808 MPU in mobile battery powered application. Can you recommend a Power Manangement IC ?
TPS650061?
TPS650061
We took a closer look at the AM1802 using the 3D X-Ray and found some opens. We built a new board last night and with a confirmed good soldering job I now see some traffic on the SD clock line as well as some traffic on the SD data line.
I need to make…
Other Parts Discussed in Thread: AM1808 , AM1802 , TPS650061 I have another post going but I wanted this one to be specific to JTAG since I'm not having much luck. I have the AM1808 eXperimenter board with the Blackhawk USB100v2 JTAG Controller. I am using…
Hello
Lower cost alternatives are TPS650006, TPS65000, and TPS650061. These are "power"only devices.
Also, TPS65073 is a more recently introduced product; it is packed with both "power" and "signal chain" resources. For…
Ueli,
The TI power team just updated their recommendation for the 34x series to the latest power converter: TPS65001
http://focus.ti.com/docs/prod/folders/print/tps65001.html
TPS650061
• Up to 90% Efficiency
• Mode Control PIN…