Part Number: TPS650250-Q1 Other Parts Discussed in Thread: TPS650250 , Hei Team,
What ESD rating of TPS650250QRHBRQ1?
Although we checked datasheet and we confirmed with TI Customer support center,we could not find any information.
Best regards.
Part Number: TPS650250-Q1 Other Parts Discussed in Thread: TPS650250 Hi team,
I could found Power-up sequencing in this datasheet. the sequence is controlled by EN pins for each DCDCs. However, I couldn't find power good pins.
would you please advice…
TPS650250 has an Operating Temperature Range of -40°C to +85°C , and a maximum Junction Temperature (TJ) of +125°C
TPS650250-Q1 has an Operating Temperature Range of -40°C to +125°C , and a maximum Junction Temperature (TJ) of +125°C …
Hi Obinna,
Thanks for providing the information! Here are the options for replacement:
From our internal cross reference tool, LMZ36002RVQT and LMZM23601 seems to be good replacements for MAXM17575ALI# and MAXM15064AMB+T respectively.
You can also take…
Part Number: TPS650864 Other Parts Discussed in Thread: TPS65023 , TPS65916 , TPS65917-Q1 , TPS6521815 , TPS650250 Hi,
my customer is using DA9062 to power xc7z007s from Xilinx.
I searched on our website and find TPS650864 suitable for artix7 Xilinx.
But I…
Yada-san,
You have two options:
Set TPS65023-Q1 LDO output voltage to 2.8V = 101b or 3.0V = 110b and test to see if either of these will work for your 2.8V requirement. 3.0V will produce 2.9V if you ensure the I*R losses in the trace from LDOx output…
Mitchell,
Yes, there is some documentation that will allow you to implement the TPS65023-Q1 without a host MCU.
The TPS650250 is a similar part that does not have any I2C communication or an internal Register Map to indicate PG and generate interrupts…
Hi Yimin,
TPS650250-Q1 can not support J5Entry low power mode (standby, sleep), as it has no I2C interface, see below e2e thread:
e2e.ti.com/.../488603
TPS659119-Q1 has I2C interface and also many other features comparing with TPS650250-Q1, so TPS659119…
Part Number: TPS650250 Other Parts Discussed in Thread: TPS54340-Q1 ,
Hi team,
Could you give me advise on following customer request? What document or material should the customer refer to?
<Customer request>
Could you tell me how to estimate power…