Part Number: TPS65381-Q1 Hi, Could you tell me about register reading during BIST? Data sheet page 31 contains the following information: "The SPI registers may be unavailable during a BIST, so no SPI reads or writes should be made while the BIST is running…
Part Number: TPS65381A-Q1 Other Parts Discussed in Thread: TPS65381-Q1 We have used the TPS65381-Q1 until now and have tested the new TPS65381A-Q1 by swapping it on an existing board.
With the TPS65381-Q1 the board started up autonomously,
With the…
Part Number: TPS65381-Q1 Hello,
One of my customer came with the following questions,
There is a maximum output capacitance requirement for the linear regulators. (5 uF Max)
For 3.3V I have a separate DCDC converter. In the meanwhile the load of…
Part Number: TPS65381A-Q1 Other Parts Discussed in Thread: TPS65381-Q1 , Dear TI team,
we have 4 PCBs which use the TPS65381-Q1.
Can we change the BOM of these PCBs to TPS65381 A -Q1 without compatibility problems?
What is the difference between…
Part Number: TPS65381-Q1
Hi, The following contents are described in the data sheet. Which Is period of the following can not be accessed by the SPI? 1.4.2msec after ”Reset→Diagnostic” 2.21msec(±5%) Could you give me your advice? Best Regards, Yusu…
Hello whong,
Is the WatchDog bit set in SAFETY_ERR_STAT register? I am not very familiar with TPS65381. Did you try the TPS driver and the example code in safety library?
Part Number: TPS65381-Q1
For software debug, I am using TPS_SetMCUSoftwareDebugMode function from sample code.
My question is when i need to exit from diag mode?
How to identity whether program is running without debugger (normal mode) or with debugger…
Part Number: TPS65381-Q1 Other Parts Discussed in Thread: RM48L952 , HALCOGEN , TPS65381A-Q1 Hello Could you help with following request
I am currently working on connecting RM48L952 dev board with TPS65381 evaluation board and wanted to ask about SPI…
Other Parts Discussed in Thread: TMS570LS20216 Hi,
I'm using the TPS65381 connected to the TMS570LS20216. My code is based on the TPS65381/RM46_NoRTOS project. I had the TPS to go to the diagnostic state and watchdog function was running with respect…