Part Number: TPS65920 Other Parts Discussed in Thread: TPS65218D0 AS the TPS65920 is NRND,what is recommended replacement for new design?
Which PMU recommended to be used for AM437?
Other Parts Discussed in Thread: TPS65920 , DM3730 Hello. I`m building DM3730 based module, I used TPS65920 as PMIC. Here is a schematics:
I made first PCB (without CPU for now), and TPS65920 did not start. The only voltage I got is 1.5V at VINTDIG…
My question is what could be done if the USB is connected to a USB HUB which do inject VBUS when the PMIC is enabled ?
Could it be forced to be an A device ?
Other Parts Discussed in Thread: TPS65920 , TPS65950 Question from the customer:
Our question is with regards to the TPS65920 OMAP Companion Chip...
We are trying to understand why we are getting ~1V back onto VBAT when 5V VBUS is applied and main…
Hi,
No there any activity at all at the DP/DM line.
The same DOK working perfect. at another project with the same omap3530 but with pmic tps65950 and not like at this project that we have here tps65920.
Thanks in advance,
Tanya
Other Parts Discussed in Thread: TPS65920 , AM3715 hello everyone,
when i used usb-lan on am3715+tps65920(usb otg),it only sends socket below 465 bytes .
if the socket over 464 bytes,it failed and if this happened ,you can't send anything,even the…
Other Parts Discussed in Thread: TPS65920 Customer is asking: I am doing an experiment with JTAG on the TPS65920. In the documentation, it says that JTAG pins are multiplexed with GPIO pins. TI doesn’t explicitly say what you need to do with the TEST…
Other Parts Discussed in Thread: TPS65920 , TEST2 Hi Team,
Could you help with the question below?
I have a question regarding JTAG in TPS65920:
What's the purpose of each of the TEST pins in the PMIC?
TEST1, TEST2, TEST3....
So…