Part Number: TDA4AH-Q1
when I flash the follow version, and the weston could not work, please help to check.
I download the bin ti-processor-sdk-linux-adas-j784s4-evm-09_02_00_05-Linux-x86-Install.bin
I follow the tutorial create-sd-card-with…
Part Number: TDA4VM-Q1
Tool/software:
Dear Sudheer,
RTOS SDK Version:10.01
As we discussed in other thread earlier,Our current requirement is to use ethfw on MCU20 and then implement inter ping within the local area network on Linux through virtual…
Part Number: TDA4VH-Q1 Tool/software: Hi Ti Team,
My debugging environment is as follows: SDK version: 10.0 SOC: TDA4VH88
Flash chip: MX25UW51245GXDR00
The hardware schematic diagram is as follows:(Although the flash shown in the schematic diagram…
Part Number: TDA4VH-Q1 Tool/software: hi,ti expert:
We found that sdk9.1 could not communicate after changing the mac address,After checking, we found that linux sent requests, carrying mac addresses are always old。
Also, the driver on the linux side…
Part Number: TDA4AL-Q1 Tool/software: Hi, Dear Expert
Because I suffer from display node created failed problem, so I try to use "basic TIDL application" to make sure Display is OK.
HW : J721S2 EVM + DISPLAY 0
SW : SDK 10.0 with default build vision…
Hello,
Thank you for your response.
Doredla Sudheer Kumar said: Can you please A72 Log? I have seen A72 client Virtual Port info is showing Mask for Switch Port 0, MAC Only Port-4 in switchport info and also virtual MAC port info also seen
Indeed…
Part Number: TDA4VH-Q1 Tool/software:
HI TI.
In my application, I observed that the C7x DSP halts during execution.
This issue seems to improve when the page cache is periodically dropped.
During the analysis, I found that the vx_app_arm_ipc…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TDA4VH start log.txt
Hello:
At present, we use Micron's MTFC128GBCAQTC-AAT chip for TDA4VH chip and SDK version 0900. During HS400 startup, EMMC speed switching fails, and the error returns …
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TDA4VH , SN65DSI86 Hi,
TI experts,
Now we are working on SDK 0900 on TDA4VH EVM board.
We are now conducting a long-stability test of the open-and-close video, and we have found that there…
Hi,
hongyao.jin said: 1.We would like to know what the differences are between this L3 MSMC MEM and L1 L2 MEM.
L1 Memory is the s mallest, fastest memory directly within each C7x core. It serves as the primary memory for instructions and data with…