Part Number: TPS65950 Hi all,
I am looking for the I2C ID5 address for TPS65950.
Pg. 25 (attached) of the TPS65950 datasheet specifies the addressed for ID1-4, but does not specify the address for ID5. ID5 is for the SmartReflex module.
Kalirajan,
Searching for "TPS65950/30/20 filetype:txt" in google led me to the following document, hopefully it is the text file in question.
Best Regards,
Rick S.
ADVANCE_WARMRESET_SEQUENCE.txt
[[
*********** TPS65950/30/20 advance…
Part Number: TPS65950 Hi,
For TPS65950, audio block, please provide a example sequence of De-initialization and initialization, when we switch between different outputs(IHF, EARPIECE, HEADSET)
Audio(mono) is coming from pcm interface routed through audio…
Part Number: TPS65950 Hi,
I have some issue about tps65950
1:VIO voltage is not right, Output voltage is 1.6V,Right maybe 1.8V,Attachement is TPS65950 SCH,Could you help me to check It,If there is a design problem.
2:Could you give me the…
Part Number: TPS65950 Hi team
I am supporting Japanese customer as FAE, please give me some advice.
TPS65950 VIO1.8V is used in customer's application, but during start-up, due to rush current, this current hits current limit twice. (they said at first…
Other Parts Discussed in Thread: TPS65950 Hi All,
We are working on TI-DM3725 and TPS65950 and facing issues with Battery HW charging, below are details:
Testing USB wall charging
Using and selecting automatic HW USB wall charging.
Charge current is set…
Other Parts Discussed in Thread: TPS65950 , DM3725 Hi All,
We are working on TI-DM3725 and TPS65950 and facing issues with Battery HW charging, below are details:
Testing USB wall charging
Using and selecting automatic HW USB wall charging.
Charge current…
Other Parts Discussed in Thread: TPS65950 HI,
What is the most preferred solution in tps65950 for a simple headset button? While pressing Headset button, it sets HSMIC_P to GND.
Is it possible to “detect button pressing” this inside of TSP65950 using microphone…
Other Parts Discussed in Thread: TPS65950 I have a customer that is using the TPS65950 in the following manner:
We currently use the USB port on TPS65950 to interface to USB-serial or USB-Ethernet device using the USB power from TPS65950 directly. Since…
Other Parts Discussed in Thread: TPS65950 , DM3725 Hi All,
We are working with TI-DM3725 and TPS65950. We are facing an issue LDO short circuit detection.
We are trying to consume power with cutting the LDOs (3V1, 1V5, 1V8) when the device enters the suspend…