Please refer to www.ti.com/.../tps65982-hiutility for examples on how to configure/program the TPS65982 via the host interface. Please also consider this application note. www.ti.com/.../getliterature.tsp
Support for TM4C123GXL is not natively provided…
Whoa, great debug work for the FTDI chip in the Python code in such a short time! Thanks for sharing the .py (.txt) file. Hopefully the team can use this to expand the capabilities of the TPS65982-HIUTILITY Tool SW.
Glad you got the FW update procedure…
Other Parts Discussed in Thread: TPS25810 , TPS65982-EVM , TPS65982-HIUTILITY Hello Team,
To use TPS65982EVM as load simulator in UFP configuration (while using TPS25810 as DFP), below are some quires.
1. We connected the Type C cable from DFP board (TPS25810EVM…
Other Parts Discussed in Thread: TPS65982 , TPS65982-EVM , TPS65982-HIUTILITY
Hi,
I will develop USB-PD with TPS65982.
In this product folder, the EVM can be operate with MSP430 launchpad.
Is there available sample code?
best regards,
kyt
Hi Manjunath,
The latest version of the TPS65982-HIUTILITY is a GUI that works with the Aardvark, USB2MANY EVM (that we are in the process of creating as an EVM), and the Flash Update over USB feature now enable in the TPS65982 or TPS65986.
If you download…
Both I2C and SPI ports should be "0" for Aardvark. It appears that the aardvark.dll file is missing from your directory. Using the TotalPhase Aardvark adaptor requires a few additional steps as outlined in section 5 of the TPS6598x Utilities Tool User…
Other Parts Discussed in Thread: TPS65982-HIUTILITY , TPS65982 ATTACHMENTS:
flash_update_fullFW_I2C_Enhanced.py
#!/bin/env python
#==========================================================================
# (c) 2015 TI
#----------------…
Hi Daniel,
How are you reading the registers? Are you using the TPS6598x Ultilities GUI?
TPS6598x Ultilities GUI:
User's Guide:
Could you verify that the the TPS6598x is a sink?
The Type-C current advertisement will depend on what it the DFP (Source…
Hi Kai,
There are 2 different ways to allow the user to update the FW on the tps65982
1) The first way is FTDI (FT4323) =>
***step by step procedure to this flash method can be found under page 11 of <www.ti.com/.../slvuar8a.pdf>
***note…
Hi Nat,
Can you tell me a little more about your set-up?
For the file you provided is that the image flashed onto the TPS65982-EVM board? If so can you tell me the source/sink capabilities of the NB that you have attached to the EVM? If you do not know…