Part Number: TPS65987DDJ Other Parts Discussed in Thread: TPS65987D Hi Technocrats,
I am using TPS65987d on my custom design board. I an using the docking station with this device, when I connect a docking station when I connect the optical mouse and keyboard…
Part Number: TPS65987DDJ Other Parts Discussed in Thread: TPS65987 , TPS65981 , , TPS55288 , TPS25750 , UCC29950 Hello:
Reading thru the TPS65987 d/s and applications for a USB C pure PD, one gets no idea about strangely named GUIs one can/must use for Configuring…
Part Number: TPS65987DDJ Other Parts Discussed in Thread: TPS65987 , TPS65987D Hi,
We are using TPS65987DDJ for UFP and ALT mode.
We are trying to load the patch bundle from Host through I2C Referenced from /cfs-file/__key/communityserver-discussions-components…
Part Number: TPS65987DDJ Other Parts Discussed in Thread: TPS65988 , TPS65987 Hi,
We have just received our product prototype which uses TPS65987DDJ on it.
We have a Linux Board connected to the PD through I2C2 lines.
I wrote a custom user space driver…
Part Number: TPS65987DDJ Other Parts Discussed in Thread: TPS65987 , TPS65987D Hi
My customer has questions as below.
Aplication: 3KW Powerbank
-Questions-
1. Is there a program installed in TPS65987 by default? If so, what programs are installed?
2. The…
Part Number: TPS65987DDJ Other Parts Discussed in Thread: TPS65987 I'd like to add a couple of parallel questions pertaining https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1186453/tps65987d-supplying-vconn…
Part Number: TPS65987DDJ Hi,
We have an ARM based Host processor which runs on Linux Kernel v5.4 and it controls TPS65987DDJ through one of its I2C lines.
The processor has an USB_ID pin input which needs to be controlled in a way that if the PD controller…
Part Number: TPS65987DDJ Hi,
We have an ARM processor based application which needs to control TPS65987DDJ through I2C lines. But the processor's IOs support only 1.8V. It was not clear to me in the datasheet whether TPS65987DDJ's I2C lines are directly…
Part Number: TPS65987DDJ
Hi,
We have an ARM based processor which control TPS65987DDJ through its I2C lines.
In our application, the PD is by default configured to have a 5V, 3A source and data role is UFP. And also we support to switch power role to…