Part Number: TPS65994AE Hi,Sir:
Need your kindly help to check how to read the PD adapter's PID and VID from TPS65994AE by SMBUS.
please give some sample code and show the relate register.
Thanks!
Part Number: TPS65994AE Hello team,
My customer wants to use the external power path (PP_EXT) as 9V/3A source.
I believe VSYS is used for reverse current protection, so I am afraid that it will go protection mode when current is sourced through PPHV…
Part Number: TPS65994AE Other Parts Discussed in Thread: TPS65994 Hi Expert,
I use the TPS65994 in a notebook application, the PD controller act as DFP_D. The description of DPConnection bit in the 0x5F DATA_STATUS register is "Asseted when there is…
Part Number: TPS65994AE Hi team,
what's the current solution (before new IC) to PD3.1 dynamic OVP?
I heard there's two ways, one is use 65994 default OVP with voltage divider on VBUS to detect 28,36 or 48V
second is use GPIO to turning on the…
Part Number: TPS65994AE Other Parts Discussed in Thread: TPS65994 Hi team,
Our pcb uses TPS65994 and want to select the I_LIM5V configure to setting parameters 0/1/2/3/4.
However, we could not find any configuration parameters on the Application…
Part Number: TPS65994AE Other Parts Discussed in Thread: TPS25750 , TPD2S300 , TPD4S311 , TPD6S300 , TPD8S300
Hi Team,
Customer would like to design PD controller.
Has TI developed the PD that is integrated with the Short-to-VBUS Overvoltage Protection…
Part Number: TPS65994AE Other Parts Discussed in Thread: TPS65994 , Hi Sir,
I didn't find the correct part number of TPS65994 BH at above select Part Number , so I chose the similar Part Number of TPS65994AE for issue discussion.
Platform: Intel RPL…
Part Number: TPS65994AE Other Parts Discussed in Thread: TPS65994 Dear Team,
Our pcb uses TPS65994 and want to know the recommend decoded value of ADCIN 1/2 and Dead battery configuration.
Our system is Battery-less design.
Which dead battery…
Part Number: TPS65994AE I am working on a USB hub board. I am connecting a USB host to a USB hub’s upstream port using a Type C cable. I have a power bank option in my USB hub.
If that power bank is connected, USB host should get charged through the…
Part Number: TPS65994AE The datasheet mentions modern standby being a "special case of the Idle mode". Two questions on that:
1) what is the difference to idle mode?
2) is any configuration needed to put the device to modern standby mode?
One more…