Part Number: TPS2597 Other Parts Discussed in Thread: TPS25948 , TPS66020 hi team,
please help recommend the DPS1113 same or function similar part?
regards,
Robin Liu
Other Parts Discussed in Thread: TPS66020 HI sir,
Pls kindly provide TI P2P solution, thanks a lot!
www.nxp.com/.../usb-type-c-cc-smart-protection:NX20P0477
Part Number: TUSB320 Other Parts Discussed in Thread: TPS66020 , Hi team. I'd like to configure TUSB320 and TPS66020. I have a question about the IDpin's configuration for TUSB320. Is the ID pin asserted Low when the DFP or the DRP is connected? I care…
Hi Daniel,
In our portfolio, we have the TPS66020, but is not bidirectional, The high voltage power path is only for sink applications.
I would recommend looking through the Power Switch portfolio to see if their is a suitable device for you. If you find…
Hi Ann,
TPS66020 is specified for 4-V to 22-V for SINK power path. For SOURCE path using the internal switch the spec is for 5V only .
It could be possible to design your system with Source path for high voltages but you will need and external switch architecture…
Part Number: TUSB320 Other Parts Discussed in Thread: TPS25750 , USB-PD-CHG-EVM-01 Hi,
In my design I have just one USB 1.1 Host-Lite port available and needs external power source (5V, 3A).
Considering this I'm exploring if there's a way to using USB…
There are different power role, data role, feature or specific application one needs to consider when designing type-C and USB Power Delivery system. Which type-C and USB Power Delivery IC from Texas Instruments to use for the application?