Part Number: TPS73101-EP Hello E2E,
Good day. Are the RθJC Junction-to-case and RθJB Junction-to-board thermal resistances of catalog part TPS731xx can be applied to TPS73101-EP (TPS73101MDBVREP)? If not, please provide RθJC and RθJB.…
Part Number: TPS73101-EP Hi,
I am wondering if the junction-to-case and junction-to-board thermal resistance values are available for TPS73101MDBVREP?
Please get back to me at your earliest convenience.
Thanks,
Sadab Bahar
Part Number: TPS73101-EP Hi,
We are planning to use your Low drop Regulator part: TPS73101-EP for our below requirement,
Input supply : +3.2 to +3.3V
Output : +3.15V
Load current : < 75mA.
1) In that condition sometimes, Output side revere voltage…
Part Number: TPS73101-EP Other Parts Discussed in Thread: TINA-TI Hello team,
I'd like to import TPS73101 to the TINA-TI. I can find PSpice models on the TI.com but not for TINA-TI model.
Thanks in advance. S.Sawamoto
Part Number: TPS73101-EP Other Parts Discussed in Thread: LM317 , LM1086 I am looking to replace an LM317 in an existing design where it is used as a constant current source.
The constant current source provides a consant 10mA to a resistive fuel sensor…
Part Number: TPS73101-EP I have a couple of questions regarding the Irev specification:
Is this only valid for fixed voltage versions of the part? So the adjustable version would not be covered by this specification?
The REVERSE CURRENT section of the…
Part Number: TPS73101-EP
Hi everyone,
I've got a question related to the TSP73101 part number. In the page 4, I've seen this table:
The question is:
Has Vin to be >= Vout + 0.5 Volts? That is to say, if I've got Vin =3Volts, Can I get Vout =…
Part Number: TDA4VM Other Parts Discussed in Thread: TPS73101-EP , TLV70018-Q1
Hello
I am curious about the difference between configuring the LDO for eFUSE power and using the LDO3 of PMIC-B.
PDN Note (v0.18)
6) SoC devices come in two types: General…
Hello,
Check out the TPS73101-EP.
You can also check out the TPS784. It has actually been tested down to -55C, as can be seen in the TC plots.
Best regards,
Nick
Part Number: TPS73133-EP Hi
TPS73101 has reverse current when Vfb is more than 1V above VIN. its Vfb reference voltage is 1.2V, if TPS73101 is set to 3.3V.
so when input voltage is 0V and output is 3.3V, at this condition, Vfb is 1.2V, so Vfb is 1.2V…