Part Number: TPS7A44 Hello,
I was looking at the datasheet for this LDO, and was wondering what the exact purpose of the MID_OUT voltage pin is. Under what conditions can this pin be left grounded if unused? Looking to connected OUT pin to a Power over…
Part Number: TPS7A44 Hi,
I want to review the schematic of MPN - TPS7A4450DGQR.
My Requirements are as follows:
Battery Input - 6-36V
Output - 5V, 25mA
Load Dump Case (65V) & Transient pulse also comes at the Input
The Input Voltage goes…
Part Number: TPS7A44 Other Parts Discussed in Thread: TPS7A43 Hi LDO team,
I would like to learn if below GPNs support bypass cuicuit.
-TPS7A44
-TPS7A43
Bypass means when Vin < set Vout, Vout will follow Vin as long as it is above the Vin…
Part Number: TPS7A44 Hi,
I designed a circuit with the TPS7A4433DGQR (3,3V fixed output.).
When the input Voltage is 20V I can draw up to 12mA on the 3.3V output before the Outputvoltage gets big bumps and soon breaks down. At 60V input I can draw…
Part Number: TPS7A4101 Other Parts Discussed in Thread: TPS7A44 , TPS7A30 , LM1085 Dear Team,
Do we have any LDO solution can meet the spec as below?
Vin=48
Vout/Iout= 28V(2A), 5V(30mA), -7.5(10mA), -3.4(10mA)
Many Thanks,
Jimmy
Other Parts Discussed in Thread: TPS7A43 , TPS7A44 Dear team,
PTPS7A4350DGQR is out of stoke. What are our most updated alternatives to this device?
Thanks,
Oded
Part Number: TPS7A16 Other Parts Discussed in Thread: TPS7A44 Hello,
I would like to check with you about a p2p alternatives for the following PN :
TPS7A1650QDGNRQ1 (the TPS7A16 parts family)
This is for future usage and currently it doesn’t…
Hi Suraj,
While it would not be as efficient, you could clamp it externally with a Zener diode. The most efficient way to do this is with the TPS7A44 . This is a 65V tolerant ultra-low Iq regulator.
Part Number: LMZ14201H Other Parts Discussed in Thread: TPS7A44 , TPS7A33 , , LMZ14202H , LMZ14203H , TPS7A47 , TPS40210 , PMP9624 Tool/software: WEBENCH® Design Tools We want to convert a +24V, GND, -24V power input to +16V, GND, -16V and fed them into…