Hello Zirui,
TPS7B87-Q1 is a good start. Is it ok if the part is not P2P?
Here is a quick comparison, in which I also added TPS7B70-Q1 if P2P is not needed.
MAX25210
TPS7B87-Q1
TPS7B70-Q1
AEC Q100
YES
YES
YES
Output Options
Adjustable Output, Fixed…
Part Number: TPS7A43 Other Parts Discussed in Thread: TPS7B82-Q1 , TPS7B63-Q1 , TPS7B70-Q1 , TPS7B4253-Q1 , TPS7B7701-Q1 Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "bd4269efj-ce2" ?…
Part Number: TPS7B82-Q1 Other Parts Discussed in Thread: TPS7A61-Q1 , TPS7B70-Q1 , TPS7B63-Q1 , TPS7A65-Q1 , TPS7B81-Q1 , TPS7A66-Q1 Hi
I would like to ask 2 questions below:
1. TPS7B8233 only supports 3.3V output and TPS7B8250 only supports 5V output right…
Part Number: TL1963A-Q1 Other Parts Discussed in Thread: TPS7B70-Q1 , TPS7A60-Q1 Hello.
My customer requested to share the CTE information of ICs below.
CTE (Coefficient of Thermal Expansion) of TL1963ADCQR(Lead Frame) .
CTE (Coefficient of Thermal Expansion…
Hi ,
Please consider TPS7B82-Q1 and TPS7B70-Q1. Both of these devices are designed to be off battery and survive battery transients.
Very Respectfully,
Ryan
Part Number: TPS7A63-Q1 Other Parts Discussed in Thread: TPS7B70-Q1 , TLE4275-Q1 Dear TI:
I have noticed the datasheet of tps7a63-q1, the input voltage range from 4-40v change to 11-40v. I was a little confused . The battery voltage always form 9-16v in…
Hi Kevin,
The minimum Vin to ensure proper operation for TPS7A61-Q1 is 11 V. With a lower Vin, there is a small chance that the output will turnoff.
Please consider TPS7B70-Q1 or TLE4275-Q1 for the most similar alternatives if a lower Vin rail is…