Part Number: TPS7H4003-SEP Other Parts Discussed in Thread: SN54SC8T541-SEP , Tool/software: Hi,
I am attempting to design converting a 2.5V Single Ended clock to 5V using SN54SC8T541-SEP (PN54SC8T541MPWTSEP) for CLK SYNCs to the TPS7H4003-SEP Regulator…
Part Number: TPS7H4003-SEP Tool/software: Hi,
Could you let me know PG timing difference between 2 parallel devices?
Customer would like to use it for parallel operation with 2 devices.
Due to some issue, they want to use PWRGD of device1 and device2…
Part Number: SN54SC8T541-SEP Other Parts Discussed in Thread: TPS7H4003-SEP
Tool/software:
Hi,
I am attempting to design converting a 2.5V Single Ended clock to 5V using SN54SC8T541-SEP (PN54SC8T541MPWTSEP) for CLK SYNCs to the TPS7H4003-SEP Regulator…
Part Number: TPS7H4003-SEP Tool/software: Hello,
The Single Event Test report for the TPS7H4003-SEP (slvk086a) shows in the test board and circuit diagram, "TPS7H4001-SEP" Additionally, the images of the die in both test reports are identical.…
Part Number: TPS7H4003-SEP Tool/software: Hello,
When using the external sync on the TPS7H4003-SEP:
1) If an external reference clock is not available within 20uS and the regulator switches to internal clocking, will the regulator switch to an external…
Part Number: TPS7H4003-SEP Tool/software: What is the reason for having parallel diodes in the buck design on the EVK? The datasheet highlights the importance of a Schottky diode to reduce noise, but gives very little info about the how & technical background…
Part Number: TPS7H4003-SEP Hi all,
I am looking into the TPS7H4003-SEP packaging, and on the datasheet, it states that the NC pins are defined as no connects. Are these pins a floating metal? If there are a floating metal, do these pins need to be tied…
Part Number: TPS7H4003-SEP HI all,
I am looking into the TPS7H4003-SEP, and I had the following questions below concerning the internal mosfets and body diodes of the device:
What are the min. tr (rise time) and tf (fall time) for high and low side…
Part Number: TPS7H4003-SEP Other Parts Discussed in Thread: TPS7H4001-SP When using the design calculator for the TPS7H4003-SEP in parallel mode, what is the correct procedure?
For instance, if the total load is 20A and a dual configuration is being…
Part Number: TPS7H4003-SEP Hi,
I'd like to know how is the TPS7H4003-SEP behavior in case the input voltage reach 10V permanently. Will the output short-circuit with the input level?
Regards and thanks in advance for your support.
Raúl