Part Number: LOWPASSFILTER-CALC Other Parts Discussed in Thread: TINA-TI I am trying to design a single-stage 2nd-order active LowPass filter. In the past I used TI Filter Pro, but it looks like that has been discontinued. I found Webench Filter Design…
Part Number: LM5069QUICK-CALC Other Parts Discussed in Thread: LM5069 Hi,
We are using LM5069-2 IC for hot swap application, below are the specs:
- Vin = 24V +/-10% tolerance
- Current Limit : 10A,
- Max load Capacitance : 2200uF
- Ta : 60C
- Power limit…
Part Number: TPSF12C1-Q1 Other Parts Discussed in Thread: TPSF12CX-DESIGN-CALC Hello,
I have a trouble with the design tool "TPSF12CX-DESIGN-CALC".
When I choose the CM choke model "1. Equivalent Circuit Model" in the Step 2, I cannot enter CM…
Part Number: TPSF12C1-Q1 In TPSF12Cx quickstart calculator Rev A2.xlsm, what's the definition of RPAR and CPAR in CM choke model. Could you draw the equivalent model to let me know the location of RPAR and CPAR?
Dear Orlando,
Out max output current is 14.5A, which is lower than 16A. We will use heatsink for heat dissipation. The Irate of inductor we chosen is 24A, which can meet the requirement.
Your reply is very helpful. Thank you very much!
Part Number: AM62X-PET-CALC Hi TI
For UG1V8_VDDA power rail , current current consumption result is Max current = 100mA, can you help assess whether this is make sense?
If the current is make sense , please help review this power rail layout design …
Part Number: FLYBUCK-FLYBACK-DESIGN-CALC Other Parts Discussed in Thread: LM5155 , LM5156 Hello, We are wondering if there is any suitable controller and circuit or calculator for the design of a flyback topology DC/DC converter that can meet the requirements…
Part Number: LM3423-Q1 Hi Team,
since Webench does not support LM3423-Q1 design anymore, can you please share your design guides and/or calculator sheets for LM3423-Q1 designs? I could not find any of them online in the product folder. It would be quite…