Part Number: TPSM8287B30 Hello,
To modeling the TPSM8287B30LAPVCHR, would it be possible to get informations about internal capacitors?
For input capacitor (22µF): effective capacitor at 5VDC, internal résistance, serial inductance for ouput capacitors…
Part Number: TPSM8287B30 Hello,
Good Day!
We are working for Thales-SIX and came across a component TPSM8287B30LAPVCHR from your website and it is suitable for our design, before proceeding to select this component we need some additional information…
Part Number: LM21215 Other Parts Discussed in Thread: TPSM8287B30 We have a design for a MPSOC using the LM21215MH/NOPB to supply the core 0.85V rail which is out for fab. The logic design for the MPSOC PL has grown significantly since the HW was designed…
Part Number: LM21215 Other Parts Discussed in Thread: TPSM8287B30 , Hello team,
My customer would like to change the current limit setting on the field.
Would it be possible to use DAC to set the current limit instead of resistor? Or should we use…
Part Number: TPS548B22 Other Parts Discussed in Thread: TPS546E25 , TPS546B25 , TPS546C25 , TPSM8287B30 , TPS6287B30 Tool/software: Dear Team,
It is found that the part TPS548B22RVFT has Lead over threshold. Please confirm if this is true and provide…
Hi Dinesh,
I dont think it would be working solution as there is no switching cycle and current control among the inductors? Device is not design for it. Device control is based on inductor current ramp.
Did you also check our module which has inbuilt…
Hi Prajesh P,
Thanks for using e2e.
For your requests please check our datasheet. The reference design and design guidelines are all provided.
TPSM8287Axx 2.7V to 6V Input, 6A, 10A, 12A, and 15A, Parallelable Step-Down Power Module With I2 C Interface…
Hi Tommy,
Thanks for the ee information.
I would recommend to change the compensation circuit to Rcomp=600 ohm, Cc1=10nF, Cc2=10pF. The rest looks good to me.
This is the calculator sheet I used: TPSM8287BComponentCalculator (2).xlsx
Since the…