Part Number: TRS213
Tool/software:
Hi
The customer received this TI TRS213 PCN.
Could you help clarify the meaning of the red box in the picture below.
Part Number: TRS213 Other Parts Discussed in Thread: MAX213 Hi,
MAX213CDBR is scheduled for EOL. I would like to know the difference from the recommended replacement TRS213IDBR.
Thanks,
Part Number: TRS213 Other Parts Discussed in Thread: SN74LVC1G34 Hi Expert,
May I know when there is no power in TRS213IDBR, what is the impedance status of TTL/CMOS output pins?
Is it pull-down or Hi-Z?
Where can I get these information? datasheet or…
Part Number: TRS213 Other Parts Discussed in Thread: MAX213 , MAX3243E , TRS3243E , TRS3243 , MAX3243 Hi Expert,
May I know the difference between MAX3243EIDBR & TRS213IDBR?
Which one has the better ESD protection?
BR,
Aaron Chen
Part Number: TRS213 Hi Team,
My customer got question that they connect V- pin to Vcc (the correct connect is connect to GND),
however they do not see issue with RS-232 communication and not difference with Tx waveform.
Customer would like check if an…
Part Number: TRS213 Other Parts Discussed in Thread: STRIKE Hello,
the TRS213 has an integrated ESD protection that works well. But we have one scenario in the field that causes the IC to burn.
The TRS213 is used to level shipft and protect all the pins…
Part Number: TRS213 Hi Sirs,
We would like use TRS213 to replace ADM213EARSZ/SSOP.
But we saw there only show P on TI cross reference, not show "S"
P: TI device has the SAME FUNCTIONALITY as the competitors device, but is not pinout compatible…
Part Number: TRS213
Dear Team,
Please help to answer below questions.
1. We used O_COM1_DTR1# as SIO Strapping function. We pull it up to 3.3V and found that there is a 2.12V leakage voltage on Vcc pin. Is there any concern? We also pull it to ground…
Other Parts Discussed in Thread: TRS213 customer would like to confirm the TRS213 behavior in abnormal application scenario below:
1) Does Rout support default state(or keep the previous state) if TRS213 working abnormal?
2) will the TRS213 burn(or crash…
Other Parts Discussed in Thread: TRS213 , SN65HVD485E Hi Sir,
Sorry to bother you.
Our end customer product is E-BOX which include RS-485/232.
We have use SN65HVD485E and TRS213
End customer would like confirm are there have any risk if they use 4-20mA…