Part Number: MAX3221 Hi team,
As I know, they are the same. TRS is the TI brand name and MAX is the generic brand name.
But the pricing is different on TI website. Max pricing better than TRS.
SoCould I suggest customers use MAX?
Part Number: TRS3221E Hello TI interface team!
I have to make up a interface adaptor containing, among other parts, a RS232 <-> RS422 conversion.
For those I have selected the abovementioned components. They are directly coupled back-to-back by…
Part Number: TRS3221E Other Parts Discussed in Thread: TRS3221
Dear TI Team:
we have TRS3221EIDBR in our design, and the SCH is attached
1. Pls help review the sch attached, Thanks
2. D oes TRS3221E need pullup on TIN and ROUT pin ? This is not mentioned…
Part Number: TRS3221 Hi,
My customer is using TRS3221 now, they want to know what's the withstand voltage requirement for the caps used on TRS3221 and what about the tolerance. Can you tell the withstand voltage and tolerance for C1,C2,C3 and C4 ?
Best…
Part Number: TRS3221 Hello,
Please tell me the difference between TRS3221CPWR and TRS3221IPWR.
"6.3 Recommended Operating Conditions" has the following description. Ta: Operating free-air temperature was as follows.
TRS 3221 C 0 to 70 ° C…
Part Number: TRS3221 Hi Sir
May we have IC can support as below spec?
Serial Ports RS-232 / RS-485 (Dual mode / Software Selectable RS-232/RS-485 ports)
RS-232è4 pin (TXD/RXD/CTS/RTS)
RS-485èFull Duplex (TXD+/TXD-/RXD+/RXD-)
…
Other Parts Discussed in Thread: TRS3221 , SN74AUP1T50 Hi,
I am using the TRS3221 in a UART application (PC -> DB9 -> TRS3221). The logic level for my device is 2.5V (3.3V input tolerant) therefore I am using a level shifter, SN74AUP1T50, only on DIN.…