Part Number: TRS3232E Tool/software: Hi SIR
I saw the TRS3232E datasheet and on the same package the data rate only 250 kbps.
Can the data rate really reach 1Mbps? or Just pin compatible.
Part Number: TRS3232E-Q1 Hello Team,
I am currently performing Signal Integrity analysis for our board, which includes the component TRS3232EQPWRQ1 . To proceed with the analysis, I require the IBIS models for this part. As it is not available on the…
Part Number: TRS3232E-Q1 Hi
Please share the charge pump frequency details for RS232 transceiver IC TRS3232EQPWRQ1
Facing issues in CE and RE test as per CISPR25 class3 failing at frequencies 530, 640, 760, 880 KHz
Part Number: TRS3232E-Q1 Hello,
Please provide the Case Temperature and Junction to case thermal resistance for the TRS3232EQPWRQ1 as I was not able to find this specification in the datasheet.
Thanks & regards, Deep Narkhede
Part Number: TRS3232E Tool/software: Hi,
I have seen this in the past from some of the RS232 transceivers in the market but, can the chip be powered when there is a +10V on the RS232 lines, while the chip is supposed to be OFF ?
Is current leakage…
Part Number: TRS3232E Tool/software: Hi,
I have a question about TRS3232EIPWR and MAX3232EIPWR.
The recommended operating range in the data sheet is VCC (min) =3V. Therefore, is it correct to understand that the IC is in the Disable state when VCC…
Part Number: TRS3232E-Q1 Other Parts Discussed in Thread: ESDS552 Hello,
We are using the TRS3232EQPWRQ1 IC for RS-232 communication. According to the datasheet, the RS-232 pins are rated as shown in the image below. Do we still need external ESD protection…
Part Number: TRS3232E Tool/software: Customer feedback that TRS3232EIPWR has different size on die as the pictures below.
Below picture#1 and #2 are from RFAB, #3 is from DFAB or CFAB? Now all material are from RFAB?