Part Number: TRS3243 Hello expert,
Could you kindly help to double check below comparison table is correct or not? Also help to fill in below empty tab? thanks a lot!
Item No.
Parameter
Original Source
New Source
3
Vendor P/N
TRS324…
Part Number: TRS3243 Hi Team,
I have a quick question about the other side of cap connection.
According to the datasheet, it can be connected to Vcc or GND, but which is better normally? When connecting to Vcc side, they have been seeing some glitch noise…
Part Number: TRS3243 I would like to use the TRS3243 IC in our existing circuit. Currently we are using the MAX3241 IC. As per the datasheet, TRS3243 is a drop in replacement IC. While testing it is not working by replacing MAX3241.
Can anyone comment…
Part Number: TRS3243 Other Parts Discussed in Thread: , MAX3243E Hi Sirs, Would you pls provide the ESD rating of IEC61000-4-2 for the TRS3243IPWR as we did on the MAX3243EIDBR for customers? TRS3243IPWR Datasheet: MAX3243EIDBR datasheet: Thank you and Best…
Part Number: MAX3243 Other Parts Discussed in Thread: TRS3243 , , TRS3243E , Hi team,
Do we have MAX3243CDBR industrial or automotive level version? Thanks!
Part Number: TRS3243E Other Parts Discussed in Thread: TRS3243 , Hi
Could you help check below the TRS3243 schematic and any need to adjust ,Thanks
TRS3243E.pdf
Part Number: TRS3243 dear sir,
what is the power consumption of TRS3243 under following conditions: Vcc=3.3V, RL=3.3KOhms, 115.2Kbit/s, all RS232 signals are used for customer application ?
thanks
Paul