Part Number: DS90LV047A Other Parts Discussed in Thread: TRSF3232 , TRS3227E , I am using the parts mentioned above to provide LVDS signaling over a long length of Cat5E cable (4 signals total). The LVDS segment seems to work well. Two of the signals…
Part Number: TRSF3232 Other Parts Discussed in Thread: MAX3232E , SN65C3232E , TRS3232E , Hi Team,
a customer is looking for a p2p replacement for MAX3232ESE with a data rate of 1000kbps.
Which device would you recommend also with regards to (long…
Part Number: TRSF3232 Hi
How should I process unused pins?
unuse pin: DIN2, DOUT2, RIN2, ROUT2
Is it enough to connect DIN and RIN to GND?
Is a pull-up / pull-down resistor necessary?
Best Regards.
sopatopa
Part Number: TRSF3232 Other Parts Discussed in Thread: TRSF3221E , Hello team,
My customer intend to use TRSF3232EIPWR, but they only need a single channel of it, they are wondering if TI has single channel part similar with TRSF3232EIPWR ?
Thanks…
Part Number: TRSF3232 Hi,
May I know where can find TRSF3232 Output Driving Current?
Due we need to connect long cable(~10m) and need to check signal quality again.
Thanks.
Regards,
Eric
Part Number: TRSF3232 HI Sir
May I know TI have RS485 to RS232 's reference design ?
Below is RS232 to RS485's reference design
/cfs-file/__key/communityserver-discussions-components-files/138/2045.RS232-to-RS485-Converter.pdf
Part Number: SN75C3232 Other Parts Discussed in Thread: MAX3232 , TRSF3232 , TRSF3232E , Hi team,
The customer has previously used MAX3232CDWΩ (MAX3232 3V to 5.5V Multichannel RS-232 Line Driver/Receiver)
MAX3232CDW => runs at speeds of up to 250…
Part Number: MAX3232E Other Parts Discussed in Thread: , TRS3232E , TRSF3232E , TRSF3232 Dear Specialists,
My customer’d like to confirm the difference between MAX3232E and MAX3232E-Q1.
I would be grateful if you could advise.
---Question
I checked…
Part Number: TRS3232E Other Parts Discussed in Thread: TRS3232 , MAX3232 , MAX3232E , TRSF3232E , TRSF3232 Hi Experts,
My customer is sleceting the 232 interface, they have selected the TPT3232E-SO3R.
I want to recommand the TRS3232EIDR or TRS3232IDR…