Part Number: TRSF3232E Other Parts Discussed in Thread: MAX232 team, my customer is migrating from MAX232 (115200 br) to TRSF3232EID in order to improve baud rate to 460800. looking at datasheet of TRSF, we reccomend C1=0.47uF and C2/3/4=0.33uF @5V while…
Part Number: TRSF3232E Tool/software: During the application process of TRSF3232EIPWR, it was discovered that when PIN 13 and PIN 8 do not receive a signal from the host (with the external wiring harness of the board connector left floating, maintaining…
Part Number: TRSF3232E Other Parts Discussed in Thread: SN65C3232E , MAX3232E , TRS3232E Tool/software: The part number TRSF3232E is declared as a 1Mbit/s RS232 transceiver, but at paragraph 9.2.1 (Design Requirements) is indicated that "• Maximum recommended…
Part Number: TRSF3232E Other Parts Discussed in Thread: TRS3232E-Q1 , TRS3232E Hi Team
There is a good new that we could DIN TI product!
1.Does TRSF3232E have Q version? I haven't seen the list on the official website, could you please provide me…
Part Number: TRSF3232E Other Parts Discussed in Thread: SN75C3232E , Hello guys,
One of my customers is using SN75C3232EDR for their current mass production. But they want to use TRSF3232ECDR or TRSF3232EIDR instead of SN75C3232EDR for the near future…
Part Number: TRSF3232E Hi Team,
My customer use TRSF3232E to test and the condition is 1Mbps speed.
But the IC temp high around 65C on room temp. RD uses another competitor ZT3232LFEN.
The device no like this issue. Would you help comment on this…
Part Number: TRSF3232E
Hi Team,
Our customer would like to know the transmitter input hysteresis value of TRSF3232EIDR. As I understand, the hysteresis value in the datasheet is for the receiver. Do we have the value for transmitter?
He also wants…
Part Number: TRSF3232E Hi,
May I know TRSF3232E if can support 6m Cable Length?
Any risk or Cable spec requirement about 6m Cable Length?
Thanks.
Regards,
Eric