Part Number: TRSF3232E Hi,
May I know TRSF3232E if can support 6m Cable Length?
Any risk or Cable spec requirement about 6m Cable Length?
Thanks.
Regards,
Eric
Part Number: TRSF3232E Hi
TRSF3232E is used in customer.
customer want to know how to choose capacitor C1, C2, C3 and C4 value?
in customer circuit, the cap value is larger than Datasheet recommend, but IC operation is good.
Part Number: TRSF3222E Other Parts Discussed in Thread: TRSF3232E , Hi Team,
My customer is evaluating our TRSF3232E and they need both the 20-pin and 16-pin version.
Since TRSF3232E is a 16-pin device, I suggested TRSF3222E for the 20-pin one.
I noticed…
Hi Jamie,
Jamie Tseng said: SN65C3232DW Or SN75C3232DW May I know the difference of 65 / 75?
As Clemen's has pointed out, the main difference is SN75 supports 0C to 70C whereas the SN65 supports -40C to 85C.
The newest/latest version of this device would…
Part Number: TRSF3232E Other Parts Discussed in Thread: MAX232 Hi,
I have a design in which the part MAX232 from MAXIM INTEGRATED was replaced by TRSF323ECDR to use 3.3V supply to IC. Whoever changed the part kept the external capacitors: C1=C2=2.2uF instead…
You can also use the TRS3232E (which is identical) or the faster TRSF3232E.
(The MAX3232E-Q1 is available only in the TSSOP package, which is currently available for the MAX3232E.)
The MAX3232E and TRS3232E are replacements for the MAX3232ESE. The SN65C3232E and TRSF3232E are replacements with1 Mbps support; the TRSF is more modern.
Other Parts Discussed in Thread: TRSF3232E , TRS3232E Hi,
We are trying to connect to a newly developed hardware module that has a TRSF3232E chip on it.
We can see data coming from the tx side but The computer screen on the serial port side reads non-sense…