Part Number: TS2PCIE412 Dear Sirs,
In my design, I have three PCIe entity interconnected: this PCIe ports works with different configurations.
The system sets the configuration only at the power up. At each power up, the PCIe ports can be interconnected…
Part Number: TS2PCIE412 Other Parts Discussed in Thread: TMUX1574 , , TMUXHS4412 Hi,
Would this kind of switching for the PCIe (gen 2) data lanes and control signals work ? The switches are not dynamically controlled, but bus is connected either-or to…
Gibson,
To determine if a signal switch is appropriate for a particular signal standard you need to look at a couple of parameters.
The first one you mentioned is the data rate. The TS2PCIE412 has a bandwidth of 2GHz. Theoretically the 2GHz bandwidth…
Other Parts Discussed in Thread: TS2PCIE412 I looking for Differential Switch of XAUI interface(3.125Gbps).
CAN TS2PCIE412 use(support) XAUI interface?
(I think that data rate is OK, but It isn't being written on a data seat.)
Best regards,
Satosh…
Matt,
1) The datasheet is unclear which inputs are differential inputs. I would assume that A0 and A1, A2 and A3, and so on and so forth are differential. This isn't clearly stated in the datasheet. Is this true?
I apologize for the confusion with…
Other Parts Discussed in Thread: TS2PCIE412 , HD3SS3412 I looking for Differential Switch of XAUI interface(3.125Gbps).
Please let me know 3-point below.
①Is there any application note or information of XAUI interface?
(I didn't find regulation specs…