Part Number: TS3A24157 Tool/software: Hi TI, This is Steve
I need to control a system which include SBC (single board computer) and battery
1.
The battery have a spst switch, after measurement
This spst, one contact is pull up 4V with 300K ohm and the…
Part Number: TS3A24157 Other Parts Discussed in Thread: TS5A623157 Hi,
in the enclose threat
https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/390098/i2c-2-1-multiplexer-application-for-ts3a24157…
Part Number: TS3A24157 Hi,
I found when P3V3_BMC_AUX = 3.3V, IN1/IN2 pull low, COM2 still have leakage ~2.0V to MCU.
But if I pull COM2 to GND, this leakage is disappear.
Do you know why may cause this leakage form COM2 to NO2?
Thanks!
Jeff
Part Number: TCA9803 Other Parts Discussed in Thread: INA226 , , TMP468 , TS3A24157 Hi,
In our current design, we are using the below components. Kindly , share the electrical characteristics, Voh (min) , Vih (min) , Vol (max) , Vil (max) for completing the…
Hi Gilgur-san,
Thank you reply.
> Is Pd a critical parameter in your application? why do you need Pd > 0.75W?
Because speaker can be driven up to 1W.
I think it is necessary to achieve both Ro and Pd.
And after looking at datasheet, I determined…
Part Number: TLV320AIC3100 Other Parts Discussed in Thread: TS3A24157 , TS5A26542 Tool/software: Hi Gilgur-san,
Thank you reply.
My request is to find lowest device that meets following specifications:
"2:1 2-channel device" used to switch speaker …
Part Number: TS3A24157 Hi,
My customer open the IBIS model ( ) in ti.com. They found the type of COM is input. Can we make it as output? So they can output the signal from these pins in simulation.
Thanks.
Part Number: TS3A24157 Other Parts Discussed in Thread: TS5A23157 Hello E2E Team,
I am looking for a chip which allows me to use same UART port (RX & TX) for connecting two different peripherals.
A low cost & small size chip is preferable. My voltage…
Part Number: TS3A24157 Hello,
We consider to use TS3A24157 but there is a possibility to apply voltage at NC, NO or COM pin when VCC is off.
I think TS3A24157 is not acceptable this condition. Is there alternative device to support this condition?
Best…
Shlomi,
I searched the switches and multiplexers e2e forum for “TS3A24157” and the first post the comes up is TS3A24157: Connection between COM and NO/NC when VCC=0v that tells you TI does not guarantee the state of this switch without a valid…